Koti
  • Belimo-verkkosivustot
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
    Deutsch

    Français

    English

    中文

    Português

    Español

    Español

    Français

    Italiano

    Nederlands

    Türkçe

    Polski

    Norsk

    Suomi

    Svenska

    English

    Magyar

    Eesti keel

    Русский

    Latviski

    Lietuvių

    български

    language.el_GR

    עִברִית

    Română

    Slovenščina

    Slovenský

    Srpski

    Mакедонски

    Hrvatski

    Shqiptare

    Srpski

  • Belimo-verkkosivustot
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
  • DE FR EN 中文 PT ES ES FR IT NL TR PL NO FI SE EN HU ET RU LV LT BG EL HE RO SL SK SR MK HR SQ BA
Koti

  1. Koti
  2. Belimo Blog

Targeting Actual Energy Usage

Julkaissut
Rick Ellul
on to, jouluk. 02, 2021 @ 02:45 ip.

When networks talk to each other, tools such as machine learning can be used to map out more innovative ways to operate buildings' thermal energy. The multi-unit residential sector is growing as urbanization is accelerating across the globe. Tenants and owners in residential buildings expect the same transparency with everything they run on their smartphones; energy usage will be no different. Therefore, more developers adopt thermal energy metering in centrally distributed hydronic systems. The convergence of the thermal energy metering and the building management system benefits both the building owner/management and the tenants. Synergizing networks to all talk to one another enables machine learning to map out more efficient ways to operate buildings' thermal energy.

 

The national standard for thermal energy metering for energy management and control in Canada is called CSA C900.3:21. CSA standard sets out the thermal energy meter construction criteria, data exchange, testing, verification, installation operation, and maintenance. In addition to the CSA standard, meters used for direct billing and allocation of energy costs must be certified by Measurement Canada. Measurement Canada accepts applications for meters that meet the European standards EN1434 or the Canadian Standard CSA900. 

 

As of July 1, 2019, all newly installed thermal energy meters used in trade must be approved, examined, and certified to meet the Act and Regulations requirements. As of January 1, 2026, meters without certification can no longer be installed. All certified thermal energy meters will have a tamperproof seal to avoid any fraudulent use that provides consumers’ confidence in the validity of the meter. 

 

Review Rick Ellul's full article in Mechanical Business Magazine to learn about targeting actual energy usage.

 

Rick Ellul is the Regional Sales Manager for Central and Western Canada at Belimo Aircontrols Canada Inc. He is also a member of the CSA 900 Technical committee for Thermal Energy Meters.

 

Merkinnät: Green Building Technology, Product Updates

Takaisin Blogiin

Aiheeseen liittyvät artikkelit

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read Lue lisää

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read Lue lisää

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read Lue lisää

Tervetuloa Belimo {{js-currentCountryName}} -sivustolle

{{js-currentCountryText}}
Ota yhteyttä Tietosuojakäytäntö Muuta tietosuoja-asetuksia
'+41 43 843 61 11
Tilaa
BELIMO Holding AG, Brunnenbachstrasse 1, 8340 Hinwil (Sveitsi)