Your browser is out-of-date!

Update your browser to view this website correctly. Update my browser now

×

Cookies: This website uses cookies. By using and further navigating this website you accept this. Detailed information about the use of cookies on this website is available by clicking on more Information. Close
Welcome to the Belimo Corporate Website.
Stay on the global site or select a regional site below.
Choose your location

Success Stories Around the World

Filter by
Building Type
Location
Product Range
Project Type
Document Type
5 Items

Promenade Galleries, Linz (Austria)

Belimo Safety Solutions are making a significant contribution to the fire protection of a special building.

At the centre of Linz, Austria, the Promenade Galleries are now located on an area of 12,000 m2 . Here, heritage-protected old buildings are skilfully combined with modern architecture, which offers a contemporary, urban living and working style as well as exclusive housing in all user spaces. For the Promenade Galleries project, six Linz companies have joined forces under the leadership of the electrical installation company ETECH as a joint venture for the entire technical building installation. In addition to the electrical installations, comprehensive networking and control technology, fire protection was also a focal point at the start of planning. In addition to European standards and directives, Austria also complies with state-specific regulations, making it one of the most progressive countries in the world in terms of fire protection. In all buildings with installed fire alarm systems, motorised fire dampers are mandatory and state of the art

Location:
Austria
Building Type:
Hotel, Office Building, Residential Building, Shopping Center
Project Type:
New Building
Product Range:
Actuators, Fire & Smoke Damper Actuators
Products:
Fire damper actuators
Products:
Smoke control damper actuators
Commissioning:
2018

Taiwan Semiconductor Manufacturing Company Limited (TSMC) - Nanjing Plant

The world's largest integrated circuit manufacturer (TSMC) chooses Belimo

Taiwan Semiconductor Manufacturing Company Limited, known as TSMC, is the world's largest integrated circuit manufacturer and the largest listed company in Taiwan. TSMC's annual total capacity reaches 4.3 million pieces of wafer. Belimo Characterised Control Valves, Damper Actuators and Fire & Smoke Damper Actuators have been selected by TSMC (Nanjing) Co., Ltd. as the only qualified products. 

The integrated circuits production process has restricted requirements on temperature, humidity and cleanliness of the plant. Therefore, precise control and execution of the HVAC system is very important. The reliability of Belimo Fire & Smoke Damper Actuators and the precision of Characterised Control Valves have received high recognition from TSMC.

Location:
China
Building Type:
Production Plant
Project Type:
New Building
Product Range:
Actuators, Valves, Characterized Control Valves (CCV)
Products:
Damper Actuator: 216 sets
Products:
Characterised Control Valves: 199 set
Commissioning:
January 2018

University of Hamm-Lippstadt, Hamm (Germany)

900 fire damper actuators integrated into ventilation concept via Modbus

After almost four years of construction, the new campus buildings at Hamm and Lippstadt (Germany) were inaugurated in 2014. The university is dedicated to the so-called 'MINT' subjects (mathematics, computer science, natural sciences and technology) and has space in its state-of-the-art laboratories, lecture halls and seminar rooms for up to 4000 students and 120 professorships for research and teaching. The campus at Hamm has in the meantime received the 'Ionic Award' for design. The contribution made to the ingenious ventilation and fire protection concept came from Belimo in the form of its BKN230-24-MOD communication and power supply units.

Location:
Germany
Building Type:
Schools/ Universities
Project Type:
New Building
Product Range:
Actuators, Fire & Smoke Damper Actuators
Products:
900 Communication and power supply units BKN230-24-MOD
Commissioning:
June 2014

Cincinnati Metropolitan Sewer District

Belimo’s EF Spring Return Actuators Serve as Economical Alternative to MS41xx Series Actuators

During the replacement process, a number of different actuators were examined and after careful consideration the decision was made to replace the failing units with Belimo’s EFX120-S N4 spring return actuators. In addition to having a NEMA-4 rating, Belimo’s EF actuators offered higher torque (270 in-lbs) in a single direct-coupled unit, and because of this, only 150 actuators were required to do the work that the 250 MS41xx units originally did (one EF unit can effectively operate a 66 sq ft damper). The cost for the more robust EF actuators was almost equal to the cost of ordering 250 M-Series actuators.

Location:
United States
Building Type:
Production Plant
Project Type:
Renovation
Product Range:
Actuators
Products:
150 EF Spring Return Actuators
Commissioning:
2012

Hagl GmbH, Gütlsdorf / Attenkirchen (Germany)

Reducing energy consumption and harmful emissions

Bringing thermal energy to where it can be used. With Belimo Energy Valve™.
It is not just the rising energy prices that is making heat recovery increasingly interesting for companies. Hagl GmbH in Gütlsdorf / Attenkirchen, which has been operating successfully for over 25 years in the sheet metal and metal processing sector with 130 employees, has shown the courage to embrace new ideas in its use of alternative energy sources and improving energy efficiency. For example, it has already installed a well system with a heat pump, a photovoltaic system, hot-water generation via an evaporation rig cast into the baseplate and built a wall heating system for heating and cooling. The latest project at Hagl is the heat recovery system on the hydraulic presses to heat the company buildings. The Belimo Energy Valve™ is largely responsible for ensuring that the volumetric flows, supply and return temperatures and energy recovery on the presses can be regulated, recorded and evaluated.

Location:
Germany
Building Type:
Production Plant
Project Type:
Renovation
Product Range:
Systems, Valves, Actuators, Sensors, Belimo Energy Valve™, Duct Sensors (Air)
Products:
Belimo Energy Valve™
Products:
2- and 3-way characterised control valves
Products:
Rotary actuators
Products:
Sensors
Products:
Belimo MP-Bus