vision2050.trendDetails.header.category

Integrated Planning, Installation, and Commissioning

Global construction labor productivity lags other industries due to fragmented planning, execution and operation, limited data exchange, and outdated progress monitoring methods. Innovative approaches such as integrated project delivery, advanced digital planning, and digital workflow management will help to streamline project execution, reducing costly rework and project delays.

Siloed Processes: Barriers in Modern Construction

Between 2000 and 2022, global construction industry labor productivity grew by less than 0.5% annually, significantly trailing the 2% productivity increase of the broader economy (72). Among other reasons, persistent inefficiencies in project management methodologies and lack of use of digital tools in planning and progress monitoring hinder progress.

Traditional construction project management methodologies often overlook the complex interdependencies between trades. Each party is expected to focus solely on their specialized tasks and pursue their own contractually defined objectives. This siloed approach leads to significant fragmentation and diverting interests not only between trades but also between the planning, the execution and operational phases of the project.

Current planning processes reflect this fragmentation. They consist of multiple disconnected activities, including architectural design, structural engineering, and mechanical and electrical planning. These activities may run sequentially or in parallel, though still being disconnected with limited data exchange between them. This disconnect in the data exchange extends project timelines and frequently leads to design conflicts, such as the installation of HVAC ducts clashing with plumbing or other building systems. Such issues are often only identified during the execution phase, requiring costly on-site adjustments. Moreover, the commissioning of building automation devices is still mostly done manually, making the process error-prone and devices not working optimally. Over the building’s 20+ year lifespan, maintenance interventions often further reduce efficiency.

Additionally, outdated progress monitoring and quality control methods impede real-time in sights, making it challenging for project managers to identify and resolve bottlenecks proactively.

In sum, these challenges often lead to inconsistencies and errors in project execution, resulting in costly rework and delays. This emphasizes the urgent need for a more integrated, digitalized approach to project planning and execution.

Between 2000 and 2022, construction industry labor productivity grew by less than 0.5%annually, significantly trailing the 2% productivity increase of the broader economy

Building More Integrated and More Digital

A more integrated and digital approach to planning, installation, and commissioning can address the previously mentioned challenges. This includes adopting new project management approaches, leveraging digital planning tools, and utilizing digital workflow management platforms.

New, more collaborative project management approaches, such as integrated project delivery (IPD), will help to align the interests of all parties in a construction project. IPD is an approach where all relevant participants are involved from the very beginning of a project, injecting their expertise and sharing both benefits and risks. This approach reduces siloed thinking, minimizes design conflicts, prevents material waste and rework, and ultimately leads to faster project delivery and lower costs (73).

Digital planning tools, such as building information modeling (BIM) or generative design, support collaborative project management approaches and will be increasingly adopted. BIM offers a digital 3D representation of a project’s physical and functional characteristics, ensuring accurate, up-to-date information and serving as a reliable decision-making foundation throughout the project lifecycle. Enhanced by AI, BIM tools can also automatically identify potential issues before they arise or increase planning efficiency and variant discussion by means of algorithm-based and automated planning. Studies show that 75% of BIM adopters report a positive return on investment. Beyond design, BIM can also model execution schedules (BIM 4D) and costs (BIM 5D), helping to keep projects on time and within budget (74). The use of BIM also paves the way for digital twins, laying the foundation for operational efficiency improvements during the installation and commissioning phases (75). Data needed for the commissioning of a device can be downloaded from a cloud-based digital twin prior to delivery, allowing devices to arrive pre-configured and ready for installation at the construction site. This reduces on-site installation times, minimizes errors, and ensures seamless integration between systems.

Finally, digital workflow management tools will improve material handling and progress tracking. These tools enable the streamlining of material flows and provide real-time monitoring of construction activities. Enhanced by technologies such as drone-supported inspections, these tools will enable more accurate progress tracking, identify potential delays, and improve transparency and accountability, allowing project teams to adapt quickly to changing circumstances.