您的浏览器版本过于陈旧!

请更新您的浏览器,以便正确浏览此网站 立即更新我的浏览器

×

Cookie: 本网站使用了 cookie。如果您使用并进一步浏览本网站,则表示您接受此条款。点击此处,即可获得有关在本网站上使用 cookie 的详细信息: 更多信息 关闭
Welcome to the Belimo Corporate Website.
Stay on the global site or select a regional site below.
选择你的位置

致力于可持续发展

Land O’Lakes Achieves Building Efficiency and Reduces Energy Consumptions

Land O’ Lakes Inc.’s corporate headquarters consists of multiple buildings, the two largest of which are a four-story, 135,000 square feet office building and a two-story, 56,000 square feet R&D facility / analytical research lab. Both buildings were constructed in 1980 and together they house roughly 1,100 employees.

The Corporate Sustainability Group began making plans to upgrade the facilities to increase efficiency and reduce energy consumption. HVAC systems were a particular area of focus because as the buildings aged they became more difficult to cool and meet the desired discharge air temperature set points (especially in the summer months). Improving occupant comfort was also a priority.

The following requirements:

  • Increase delta T in chilled water coils to their design specifications and achieve energy savings through increased pumping efficiency.
  • Improve occupant comfort, particularly in the summer months.
  • Gain visibility into the operation of air handlers and chilled water coils. In recent years, the chilling plant had been unable to cool the facility adequately. Energy officials at Land O’ Lakes, Inc. wanted to determine if that was due to insufficient chilling capacity or inefficiency at the building level.

The solution the Belimo Energy Valve™, a two-way pressure independent control valve that optimizes, documents and proves water coil performance.

Visit Regional Website for More Information