Home
  • Belimo Websites
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
    中文

    Português

    Español

    Español

    Français

    Italiano

    Nederlands

    Türkçe

    Polski

    Norsk

    Suomi

    Svenska

    Englisch

    Magyar

    Eesti keel

    Русский

    Latviski

    Lietuvių

    български

    language.el_GR

    עִברִית

    Română

    Slovenščina

    Slovenský

    Srpski

    македонски

    Hrvatski

    Shqiptare

    Srpski

  • Belimo Websites
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
  • DE FR EN 中文 PT ES ES FR IT NL TR PL NO FI SE EN HU ET RU LV LT BG EL HE RO SL SK SR MK HR SQ BA
Home

  1. Home
  2. Belimo Blog

Isolation of Chillers and Bypass in Closed Cooling Tower

Veröffentlicht von
Joseph Carcare
am Do., Feb. 10, 2022 @ 09:34 nachm.

Cooling towers are critical for electric power generation and even air-conditioning needs in industrial manufacturing. They are enclosed, steady-flow devices for cooling water by evaporation through direct air contact. Cooling towers use water to extract waste heat from a system and eject it into the atmosphere primarily through evaporation. The cooling tower along with the recirculating pump and heat exchanger make up a cooling system. The water will first pass through a heat exchanger, where it absorbs the heat. Water is distributed over the top of the cooling tower, and air passes over it, causing the water to evaporate. The heat is transferred from water to the air stream, raising its temperature and relative humidity to 100%. This warm air is discharged into the atmosphere, resulting in a cool water stream. The cooled water is pumped back through the heat exchanger; the cycle is repeated.

Illustration example only; required components such as expansion vessels, safety valves, etc. are not shown.

Motorized open/close butterfly valves are responsible for the isolation of the various chillers. Depending on cooling requirements, one, two, or three chillers are in operation. Manual open/close butterfly valves isolate the pumps, chillers, cooling towers, and strainers during commissioning or maintenance. The 3-way control butterfly valve (diverting valve) performs temperature control on the cooling tower so that the downstream entry temperature on the chillers is not too low. The differential pressure sensors monitor the differential pressure of the pumps to ensure the pumps are functioning and to avoid irregular operating states (cavitation, air in the system, etc.). Differential pressure sensors monitor the strainers to detect contamination in the pipe system early.

The static pressure sensors detect leakages in the system. In most cases, the volumetric flows of the generator (chiller) and consumer (usually partial load) will vary, meaning that a hydraulic separator or a buffer tank is used for the required load equalization. In addition to HVAC systems, thermal power plants, petroleum refineries, petrochemical plants, food processing plants, cooling towers are an inexpensive and reliable way of removing heat.

 

Learn about Belimo’s butterfly valves.

Kennzeichnungen: Retrofit Solutions, Technical Tips

Zurück zu Blog

Verwandte Artikel

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read Mehr erfahren

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read Mehr erfahren

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read Mehr erfahren

Willkommen bei Belimo {{js-currentCountryName}}

{{js-currentCountryText}}
Kontakt Datenschutzerklärung Datenschutzeinstellungen verwalten
'+41 43 843 61 11
Anmelden
BELIMO Holding AG, Brunnenbachstrasse 1, 8340 Hinwil (Schweiz)