Koti
  • Belimo-verkkosivustot
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
    Deutsch

    Français

    English

    中文

    Português

    Español

    Español

    Français

    Italiano

    Nederlands

    Türkçe

    Polski

    Norsk

    Suomi

    Svenska

    English

    Magyar

    Eesti keel

    Русский

    Latviski

    Lietuvių

    български

    language.el_GR

    עִברִית

    Română

    Slovenščina

    Slovenský

    Srpski

    Mакедонски

    Hrvatski

    Shqiptare

    Srpski

  • Belimo-verkkosivustot
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
  • DE FR EN 中文 PT ES ES FR IT NL TR PL NO FI SE EN HU ET RU LV LT BG EL HE RO SL SK SR MK HR SQ BA
Koti

  1. Koti
  2. Belimo Blog

Can My Building Save Energy by Retrofitting the HVAC System?

Julkaissut
Jason Tables
on to, elok. 14, 2025 @ 04:09 ip.

Retrofitting an HVAC system is one of the most effective ways to reduce energy use in commercial buildings without replacing the entire system. Many older buildings still rely on pressure-dependent control, a traditional strategy that tends to result in unstable flow, inefficient heat transfer, and higher energy use over time. By upgrading these components with retrofit-ready technologies like Belimo’s Energy Valve, EPIV, or ZIP Economizer, buildings can achieve measurable improvements in efficiency, comfort, and control. These solutions support pressure-independent operation, stabilize delta T, automate ventilation, and help reduce unnecessary strain on pumps and chillers. The result is lower HVAC energy consumption and steady progress toward energy efficiency and sustainability goals. In addition to valve and actuator upgrades, retrofits can also include replacing outdated pneumatic actuators with modern electronic ones, which offer greater accuracy and quicker response. Room and duct sensors that measure temperature, humidity, and CO₂ also contribute to better indoor air quality and energy efficiency by enabling more precise control strategies.

How often should a commercial HVAC system be replaced?

Most commercial HVAC systems are designed to last between fifteen and thirty years, depending on maintenance and usage. That said, age alone isn't the best metric. If your building is experiencing rising energy costs, difficulty maintaining comfort, or complaints about air quality, it may be time to consider a commercial HVAC retrofit. Rather than replacing the entire system, retrofitting can target underperforming components with energy-efficient HVAC solutions that lower operating costs and reduce emissions. Belimo RetroFIT+ is designed to support this approach by offering a wide range of actuators, valves, and sensors that improve performance without the need for full system replacements. RetroFIT+ also includes direct-mount solutions for replacing competitive brands, making it easy to upgrade aging components across a wide variety of systems.

What retrofit strategies are best suited for different types of buildings?

Retrofit opportunities vary based on the building’s existing infrastructure. For older buildings with two-way pressure-dependent valves, upgrading to pressure-independent technology like Belimo’s Energy Valve or EPIV can immediately reduce energy waste. Buildings that rely heavily on outside air for ventilation or operate older rooftop units can benefit from adding a ZIP Economizer, which reduces mechanical cooling demand by using outdoor air for free cooling when conditions allow. A comprehensive energy audit is the best way to determine what changes will have the most impact. It is also important to evaluate valve sizing. Many older systems suffer due to oversized or undersized valves, which contribute to inefficiency and poor system response. Identifying and correcting these sizing issues can significantly improve flow stability and energy efficiency.

What are the most effective ways to improve the efficiency of older commercial HVAC systems?

One of the most effective strategies is to upgrade the control side of the system. Upgrading older pressure-dependent control valves to advanced pressure-independent models improves both flow control and heat transfer. Actuator upgrades can also help, particularly if switching from pneumatic to electronic control, which improves positioning resolution and reduces hysteresis. Integrating smart devices that offer real-time data and diagnostics, such as Belimo’s Energy Valve with cloud connectivity, improves visibility into system operation and supports predictive maintenance. These tools can help identify mechanical issues such as valve leakage or hydronic system issues that might otherwise go unnoticed. When paired with modern sensors and networked building automation systems, these upgrades create a highly responsive, energy-efficient system that is easier to maintain over time.

What is the return on investment (ROI) for energy-efficient HVAC upgrades?

ROI depends on the building type, climate, and existing system performance. However, many Belimo retrofit customers report payback periods of just one or two years. This is largely due to reduced HVAC energy consumption in commercial buildings, lower maintenance needs, and extended equipment life. Solutions like the Energy Valve also help qualify for utility rebates and incentives, which can shorten payback time further. The ability to isolate and resolve system inefficiencies through built-in diagnostics also contributes to long-term savings by preventing failures and minimizing downtime.

What is the most energy-efficient HVAC system for commercial buildings?

There is not a one-size-fits-all answer, but the most energy-efficient HVAC systems are those that use real-time data to adapt to demand, maintain tight control of flow and temperature, and optimize energy use automatically. Upgrading to energy-efficient HVAC solutions like Belimo’s EPIV or Energy Valve, which combine flow measurement, control, and monitoring in a single package, allows commercial buildings to precisely regulate water flow and maintain optimal system performance under varying load conditions. These solutions help maintain design delta T, improve hydronic balancing, and eliminate the need for separate control and balancing valves.

How can retrofitting an HVAC system improve indoor air quality?

Retrofitting an HVAC system improves indoor air quality by enhancing control over both ventilation and conditioning. One of the most effective strategies is upgrading outdated ventilation logic with solutions like Belimo’s ZIP Economizer. This retrofit-friendly device intelligently automates the use of outdoor air, which reduces compressor runtime, lowers energy costs, and increases fresh air intake. It also ensures compliance with current ventilation codes and helps implement demand-controlled ventilation strategies.

In addition to economizer upgrades, replacing aging components such as leaking or worn-out valves helps restore intended system operation. Pressure-independent valves improve coil performance by delivering stable flow, which helps maintain consistent temperature and humidity levels. This stability minimizes conditions that contribute to discomfort, condensation, or uneven air distribution. Combined, these upgrades reduce the likelihood of thermal drift, uncontrolled bypass, or stale air, all of which can degrade air quality. By addressing both airside and hydronic control, retrofits offer a cost-effective path to healthier indoor environments.

Do energy-efficient HVAC upgrades extend benefits that go far beyond mere cost savings?

Yes, especially in terms of decarbonization, tenant satisfaction, and equipment longevity. Reducing HVAC energy consumption in commercial buildings directly cuts greenhouse gas emissions. Upgrades also support better comfort and fewer occupant complaints. Smart solutions like the Energy Valve provide performance transparency, helping facility managers diagnose issues quickly and optimize operations over time. These improvements also make it easier to meet corporate Environmental, Social, and Governance (ESG) benchmarks and sustainability reporting requirements.

Are there tax incentives, rebates, or grants available for upgrading commercial HVAC systems?

Yes, many local utilities and government agencies offer rebates for commercial HVAC energy efficiency upgrades. These can cover a portion of the cost for replacing outdated equipment or implementing new technologies that reduce energy usage. Belimo’s RetroFIT+ products often qualify for these programs. In some cases, completing an energy audit or having a decarbonization plan in place can make it easier to qualify for state or federal funding.

Is retrofitting a commercial HVAC system worthwhile?

Retrofitting is often more cost-effective than full replacement and can bring significant improvements in HVAC energy efficiency. By upgrading to pressure-independent control solutions, building owners can reduce energy consumption without major disruption to daily operations. Belimo’s Energy Valve and EPIV are engineered specifically for retrofits that move from pressure-dependent to pressure-independent systems. These upgrades allow better control of chilled water flow, reduce over-pumping, and ensure stable delta T performance. When combined with right-sized valves, modern electric actuators, and sensor upgrades, the benefits extend across comfort, energy, and operational metrics. Retrofitting remains one of the highest-impact strategies available for improving long-term building performance.

For more information about how Belimo supports energy-efficient commercial HVAC retrofits and helps reduce heating and cooling costs in large commercial spaces, visit Belimo’s Retrofit Solutions.

Merkinnät: Energy Valve, Electronic Pressure Independent Valves (EPIVs), Retrofit Solutions, ZIP Economizer

Takaisin Blogiin

Aiheeseen liittyvät artikkelit

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read Lue lisää

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read Lue lisää

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read Lue lisää

Tervetuloa Belimo {{js-currentCountryName}} -sivustolle

{{js-currentCountryText}}
Ota yhteyttä Tietosuojakäytäntö Muuta tietosuoja-asetuksia
'+41 43 843 61 11
Tilaa
BELIMO Holding AG, Brunnenbachstrasse 1, 8340 Hinwil (Sveitsi)