Thermal Energy Meter Activation

  1. בית

Qualification for activation of Belimo's Thermal Energy Meters

The thermal energy meter meets the requirements of CSA C900 and EN1434 with type approval according to the Measurement Canada AV-2478-C and European Measuring Instruments Directive MID 2014/32/EU (MI-004).

Belimo's thermal energy meter is a multi-function device that can function as a heat meter, cold meter, or heat/cold meter. The meter can be installed in the system's supply or return. With the Belimo Assistant App, users choose the position during commissioning, known as activation. The authorized specialist who activates the thermal energy meter requires a Belimo Cloud account with additional authorization obtained through an online learning module. Activation of the thermal energy meter is carried out only once and is irreversible. It is essential to be attentive and mindful during activation. If activated incorrectly, the device will measure incorrectly and must be removed and replaced at the user's expense.

If you want to be authorized to activate thermal energy meters, please follow these four steps:

1. Read Operating Instructions

The operations manual will provide guidance and understanding to perform the functions correctly and efficiently.

  • belimo_tem-mid-operations_manual_en-us.pdf (pdf - 4.31 MB)

2. Belimo Cloud Account

Sign up for a Belimo Cloud account.

  • https://cloud.belimo.com/

3. Complete Learning Module

Complete this short online learning module and aptitude test to prepare for commissioning and activation.

  • Learning Module

4. Gain Authorization

After successful completion of the learning module, authorization to the Belimo Cloud account to qualify you to activate thermal energy meters.