Belimo Establishes Foundation to Reduce CO2 Emissions From Buildings

With the establishment of the "Belimo Climate Foundation," Belimo is supporting non-profit institutions and non-governmental organizations in reducing CO2 emissions from their buildings. This raises awareness of the great leverage that building renovations have in achieving climate targets.

As an innovation-driven cleantech company, Belimo has set itself the goal of further reducing its emissions. Today, Belimo field devices already offset the CO2 emissions generated during production and operation 24 times over through savings in their application. In addition, Belimo continuously invests in projects to reduce its own emissions. To offset the remaining emissions (according to the GHG Protocol: Scope 1, Scope 2 and air travel), Belimo has established the "Belimo Climate Foundation." The purpose of the Foundation is to contribute to the reduction of CO2 emissions from buildings and to make society aware of the great leverage that building renovations have with regard to achieving climate targets.

By establishing the Foundation, Belimo is consistently pursuing its path to increase energy efficiency and to reduce CO2 emissions from buildings. "Through projects financed by the Foundation, we can optimize buildings in the area of heating, ventilation and air conditioning technology and thereby reduce the CO2 footprint of the global real estate portfolio," says Reto Wälchli, Managing Director of the Foundation. "Most people are not aware of the huge leverage the real estate sector has in achieving climate targets, and unfortunately it has been addressed far too little to date," Wälchli continues. "We want to change this with the 'Belimo Climate Foundation'."

> Read the complete Press Release by using the below link.

  • Press Release - September 05, 2022 - Belimo establishes foundation to reduce CO2 emissions (pdf - 436 KB)