2. Belimo Blog

Adapting to the Future: How the Belimo EPIV is Revolutionizing Data Center Cooling

blogs.blogArticlePage.publication.label

Modern data centers are facing a critical challenge as they grapple with ever-increasing heat densities brought on by the proliferation of computationally demanding applications such as artificial intelligence, high-performance computing (HPC), and cryptocurrency mining. These applications drive the need for advanced cooling solutions that can adapt to rapidly changing requirements. As traditional air-based cooling systems struggle to keep pace with these technological advancements, the data center industry is increasingly shifting toward liquid cooling to manage the heightened thermal loads more effectively. This shift highlights the increasing demand for innovative solutions that provide both flexibility and efficiency in cooling systems.

The Belimo Electronic Pressure Independent Valve (EPIV) is unique in its ability to meet these challenges. It is specifically designed to manage and regulate fluid flow with unparalleled precision, making it particularly suited to the dynamic environments of modern data centers.

This article is the second installment in our ongoing blog series on modern data center cooling, where we continue to explore the key challenges and innovative solutions shaping the future of IT infrastructure management. Join us for a 20-minute prerecorded webinar to dive deeper into the EPIV's role in optimizing data center cooling strategies. Click here to view the webinar and gain valuable insights into this critical aspect of data center operations.

The Belimo EPIV is an advanced flow control solution that combines a high-precision characterized ball valve, an ultrasonic flow meter, and a durable, high-performance actuator. This integration allows the EPIV to maintain precise and consistent flow rates, even as system pressures, loads, and fluid temperatures fluctuate. Introduced in 2010 and now in its fourth generation, the EPIV has been continually refined to meet the evolving cooling needs of modern industries. Its proven reliability and adaptability make it especially valuable for data centers as they adopt liquid cooling strategies.

In today’s data centers, where heat densities are rapidly increasing, predicting future cooling needs is a complex task. The uncertainty surrounding future heat loads poses significant challenges for data center design and operation. This unpredictability demands a cooling solution that not only meets current requirements but is also capable of adapting to future demands. The Belimo EPIV excels in this regard, offering unmatched flexibility through its ability to reprogram the maximum flow rate (Vmax) as needed. Unlike traditional mechanical valves, the EPIV’s electronic characterization allows the flow curve to be recalculated each time Vmax is adjusted, ensuring optimal performance and maintaining valve authority.

This ensures that the valve operates within its optimal range, providing precise control even as cooling demands change. For data centers, this means that a single EPIV can accommodate a wide range of flow requirements over time, making it an ideal solution for liquid-cooled server racks that may need to scale from 10 GPM today to as much as 25 GPM in the future. As new hardware such as GPUs are introduced and heat loads increase, the EPIV can adapt to meet these new demands, ensuring consistent and efficient cooling.

In addition to its flow control capabilities, the EPIV offers significant advantages over traditional mechanical solutions. While a simple valve and flow setter might initially appear to offer similar functionality, the EPIV’s integrated flow meter provides real-time flow feedback, delivering a level of system transparency that is unmatched by mechanical devices. This transparency allows for precise monitoring and verification that each rack is receiving the exact flow it requires. Furthermore, the EPIV’s networkability through BACnet and Modbus protocols enables remote reprogramming, significantly reducing the time and labor required to adjust flow rates across multiple racks. In contrast, traditional flow setters require manual adjustment at each valve, a labor-intensive process that becomes increasingly impractical as data centers scale.

In conclusion, the Belimo EPIV represents a groundbreaking solution for modern data centers, addressing the critical challenges posed by rising heat densities and the shift toward liquid cooling. Its ability to deliver precise, repeatable flow rates, combined with its flexibility to adapt to future cooling needs, makes it an indispensable tool in a rapidly changing market. As data centers continue to evolve, the EPIV’s advanced capabilities and ease of integration position it as a key component in ensuring efficient and reliable cooling, safeguarding the performance and longevity of today’s most demanding IT infrastructures.

blogs.blogArticlePage.topics.label

blogs.blogArticlePage.homeLink.label

blogs.relatedPosts.title.label

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read blogs.list.item.readMore.label

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read blogs.list.item.readMore.label

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read blogs.list.item.readMore.label