2. Belimo Blog

How Do Belimo Damper Actuators, Control Valves, and Sensors Integrate with a Building Management System (BMS)?

Published by
Jason Tables
on Enj, maj 21, 2026 @ 04:23 e pasdites

A building management system, or BMS, depends on accurate field-level data and reliable control. That is where Belimo devices fit into the HVAC system. Belimo damper actuators, control valves, and sensors are installed at the points where air, water, temperature, and pressure are actually being controlled or measured. When these devices are integrated with the BMS, the system can monitor, analyze, and respond to real-time field-device conditions instead of simply sending a control signal. Products such as the Belimo Energy Valve and Thermal Energy Meter can provide flow, temperature, power, and energy data for more detailed system visibility. The term BMS is closely related to BAS, or building automation system, and the two are often used interchangeably in HVAC controls.

What is a building management system?

A building management system is the software and control platform that helps operators monitor and manage building systems from a central interface. In HVAC, that can include viewing system conditions, adjusting schedules, responding to alarms, and tracking performance trends.

How do HVAC devices interface with a BMS?

HVAC field devices can interface with a BMS/BAS through hardwired signals, such as 0-10 V or 4-20 mA, digital communication, or a combination of both. The available options depend on the specific product and supported protocols, controller architecture, and system design. Control data carries commands to the device, while monitoring and diagnostic data reports operating conditions back to the BMS/BAS. Depending on the device type and integration design, digital communication can support control commands along with operational feedback, device-level diagnostics, monitoring, alarming, verification, and optimization.

What protocols do Belimo devices support for BMS/BAS integration?

Protocol support varies by product model and integration architecture. Select Belimo connected devices support BACnet, Modbus, MP-Bus, M-Bus through a converter, or standard analog signals. For example, the Belimo Energy Valve and Thermal Energy Meter support BACnet IP, BACnet MS/TP, Modbus TCP, Modbus RTU, Belimo MP-Bus, and M-Bus with the use of a converter.

What is the difference between BACnet IP and BACnet MS/TP?

BACnet IP communicates over an IP network, while BACnet MS/TP communicates over an RS-485 serial network. Both can be used in BAS/BMS integration, but they fit different network architectures. BACnet IP is common where devices are connected through Ethernet-based building networks and may require additional coordination with IT teams around network addressing, segmentation, access, and cybersecurity requirements. BACnet MS/TP is often used for field-level device networks. The right choice depends on the project’s controls design, controller capabilities, wiring approach, and IT/network requirements.

What is the Belimo Energy Valve and how does it integrate with a BMS?

The Belimo Energy Valve combines a pressure independent characterized control valve, flow measurement, supply and return water temperature measurement, energy monitoring, Delta T management, and communication. Depending on the configuration, it can communicate through BACnet IP, BACnet MS/TP, Modbus TCP, Modbus RTU, Belimo MP-Bus, analog control, and M-Bus through a converter. It can provide data for hydronic control, billing, monitoring, commissioning verification, Delta T optimization, fault detection and diagnostics, and system performance improvement.

What kind of sensor data can Belimo devices provide to a BMS?

Belimo sensors provide real-time HVAC operational data used by the BMS/BAS for monitoring, control, alarming, diagnostics, and system optimization. On the water side, Belimo pipe sensors and hydronic sensors can measure values such as flow, temperature, pressure, differential pressure, condensation, and leak detection in heating and cooling applications.

Room sensors measure temperature, humidity, and CO2 for comfort and indoor air quality monitoring. Depending on the model, Belimo room sensors can use analog outputs, digital communication through Modbus, BACnet, or MP-Bus, relay outputs, or passive temperature elements.

Duct sensors cover measurements such as temperature, humidity, enthalpy, dew point, CO2, VOCs, pressure, and low temperature limit detection. Belimo duct and air quality sensors can use analog outputs or digital communication through BACnet and Modbus, depending on the sensor type.

Belimo gas monitors can measure gases such as CO, NO2, CO2, and refrigerants, depending on the model, and can support ventilation control strategies in applications such as parking garages or mechanical rooms. Select gas monitor models can integrate into the BMS through BACnet MS/TP, while relay or analog outputs can be used to control ventilation equipment directly. Belimo gas monitors also use CAN bus communication for standalone operation and networking of multiple devices.

Why does digital integration matter during installation and commissioning?

During installation and commissioning, digital integration can support system integration, flexible control, and efficient setup. Networked BACnet or Modbus field devices can help reduce the need for traditional home-run wiring to dedicated controller inputs and outputs, depending on the project requirements and BAS architecture. System integrators can set up, monitor, and control connected devices through existing industry software, helping reduce wiring complexity, limit errors, and shorten commissioning time.

What cybersecurity or network considerations apply to IP-connected BAS devices?

IP-connected BMS/BAS devices should be coordinated with the project’s controls and IT requirements to help prevent unauthorized access, unwanted control changes, and unnecessary exposure of connected HVAC devices. For BACnet IP or other IP-based connections, teams should confirm network addressing, segmentation, access permissions, remote access requirements, and any cloud or web server settings that apply to the device and system architecture. These decisions matter during commissioning because secure communication paths help the BMS/BAS monitor, control, and maintain connected devices without creating avoidable network risk.

Why is BMS integration important for HVAC system performance?

Belimo products bring field-level HVAC data and control into the building management system. Damper actuators, control valves, sensors, and energy measurement devices contribute information that helps the BMS/BAS monitor operation, support diagnostics, and improve system performance. When properly integrated, these devices give operators a clearer view of the HVAC system and better tools for managing comfort, efficiency, and reliability.

Are you looking for HVAC training? Belimo offers unlimited access to a library of high-quality, current, and engaging HVAC video tutorials from industry experts.

Tags: Sensors, Damper Actuators, Energy Valve

Back to Blog

Related Articles

Butterfly Valves, Energy Valve, Electronic Pressure Independent Valves (EPIVs)

What is a Control Valve?

Control valves are at the heart of any modern HVAC system, shaping how energy moves and how comfort is maintained...

5 minute read Read More

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read Read More

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read Read More