2. Belimo Blog

What is CV, and How Do I Calculate It?

Published by
Aaron Nobel
on Mër, qer 30, 2021 @ 05:22 e pasdites

Valve Flow Coefficient (Cv) is the flow capability of a control valve at fully open conditions relative to the pressure drop across the valve. It is defined as the volume of water (GPM in the US) at 60°F that will flow through a fully open valve with a pressure differential of 1 psi across the valve. It is useful to know how to calculate Cv because it is the standardized valve sizing and selection method for control valves used throughout the HVAC industry.

The equation used to find Cv is 

Q = Flow in Gallons per Minute

G = Specific gravity of fluid (estimated as 1 for water systems)

ΔP = Differential pressure over valve (delta P) – stated in psi

With this knowledge, we can quickly identify that a valve with a Cv of 10 will flow 10 GPM of water at 1 psi pressure drop across the valve without any math. A practical example, if we wanted to calculate Cv to select a valve for 10 GPM flow with a required ΔP of 4, first find the square root of the ΔP √ 4=2, and use that to divide the flow of 10 GPM 10/2 = 5, which results in a Cv requirement of 5. The master specifications of a job plan will typically list the differential pressure to use when calculating Cv. In the absence of this information, a ΔP range for selecting control valves for water coils of 3-5psi has evolved. 

When selecting valves, choose the closest to the calculated Cv, typically rounding down unless a specified maximum ΔP of a project is exceeded. An oversized valve may cause control issues such as hunting or poor heat transfer (delta T) across a coil due to overflow. Conversely, an undersized valve may not provide enough flow and exceed available ΔP. 

To easily size and select valves sizing and selection, click here to download SelectPro™. SelectPro provides distributors, contractors, and specifying engineers the ability to choose valves, actuators, and sensors for their projects based on technical information, such as application, medium, torque, flow rate, differential pressure, trim materials, and other options in its database. SelectPro provides a fast, user-friendly, and flexible means for:

•           Calculating control valve cost for any size project

•           Generating valve/actuator submittal data for project

•           Printing project data and pricing

•           Exporting project data and selected products to Excel data format

•           Saving projects for future editing or ordering

•           Automatically uploading data through the web interface for easy ordering

Tags: Online Learning Resources & Tools, Technical Tips

Back to Blog

Related Articles

Technical Tips

What are Valve Pressure Ratings?

The sizing and selection of Control Valves have considerations beyond the flow capacity (Cv) relating to conditions they will encounter in operation.

2 minute read Read More

Butterfly Valves, Energy Valve, Electronic Pressure Independent Valves (EPIVs)

What is a Control Valve?

Control valves are at the heart of any modern HVAC system, shaping how energy moves and how comfort is maintained...

5 minute read Read More

Green Building Technology, Electronic Pressure Independent Valves (EPIVs), Technical Tips

How Does the Energy Valve Respond to Low ΔT and a Call for Additional Heat Transfer?

Learn how to reduce the flow to bring ΔT back to the setpoint and how the temperature setpoint for the...

2 minute read Read More