• RetroFIT+ Partners
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
    Türkçe
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
  • TR EN
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
    • RetroFIT+ Partners
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
Belimo highlights

  1. Home

Highlights

Success Story Loxone Campus, Austria

At the centre of intelligent building automation – A showcase project for learning and experiencing

Founded in 2009 in Kollerschlag, Austria, the company's mission is to use automation to create more energy-efficient, comfortable and safe buildings. Built in 2023 in the same place the company itself was founded, the purpose of the Loxone Campus is to make it possible to experience the building automation of tomorrow, today. The 15-hectare complex includes a hotel with a wellness centre, an auditorium, a restaurant, multiple office spaces and warehouses.

  • Learn more

Maximise your building’s efficiency with RetroFIT+

From smart upgrades to innovative HVAC technologies, our RetroFIT+ event showcases real-life success stories and practical approaches to retrofit projects. 

  • Discover how retrofitting can transform existing HVAC systems
  • Gain valuable insights from experts, providing you with the knowledge to make informed decisions for your business
  • Achieve your sustainability goals with ease and confidence
  • Read more
  • FAQ on RetroFIT+

HVAC air quality sensors for a healthy and efficient indoor climate

Our HVAC air quality sensors offer accurate measurements and an aesthetic and timeless design for architects, quick mounting for installers, easy commissioning with a smartphone for system integrators, and a comfortable and healthy room climate for occupants. With or without an ePaper touch display, they monitor and control multiple parameters necessary for indoor comfort and safety, including temperature, humidity, and CO2 levels. The room operating units with virtual displays allow complete and easy control without worrying about unauthorized access.

  • Read more

Riding the tide of climate change

Sustainability and energy-efficient buildings are hot topics in modern architecture, and one of the latest marvels is the Floating Office in Rotterdam. The building consists of coupled blocks of concrete that float atop the Nieuwe Maas river and uses its waters for both cooling and heating. In addition, it has smart HVAC technology from Belimo to help create an optimal environment while using minimal energy. Together with the solar cells installed on the roof, this innovative set-up makes the building entirely self-sufficient.
 

  • Read more

Belimo's lighthouse project in India

The Mumbai hub, our 3,800 square metre Indian headquarters, was first conceptualised in 2016 as part of our 2030 accelerated growth strategy. The building, built as a showcase for state-of-the-art HVAC solutions and sustainable design, was an exciting opportunity to design an eco-friendly structure from the ground up.

The building comprises office and factory space, including a Belimo customer experience center, created to actively support the customer journey toward creating healthier indoor comfort with less energy. It also offers OEMs and academics a venue to collaboratively design, build, and test the next generation of Belimo products.

  • Read more

Comfortable and healthy indoor air with room sensors and room operating units

Belimo room sensors and room operating units are designed to complement the existing sensor range. Their simple, clear aesthetics are ideal for installation in visible areas, featuring an elegant design and shallow depth that perfectly blends with the surroundings. With the expansion of the product range for visible areas of the room, Belimo offers architects an aesthetic and timeless design, installers quick assembly, system integrators easy commissioning with a smartphone and end customers a comfortable and healthy room climate.

  • Read more

Mastering the flow with Belimo Energy Valve™

Years of expansion at the Ludmillenstift Hospital resulted in an HVAC system that just could not cope. The introduction of Belimo Energy Valves™ significantly reduced the water flow rate of the heating network, resulting in smart, transparent, and energy-efficient load-dependent heating and cooling systems – while improving comfort and keeping energy consumption stable.

  • Read more

One of 1000 solutions to change the world - Solar Impulse Foundation

In the air, Solar Impulse proved that by using and rethinking existing technologies, a solar-powered airplane can fly through the night using a renewable energy source. In buildings, the Belimo Energy Valve™ rethought the control valve to not only control flow but also control power and manage delta T, delivering transparency and ensuring energy-efficient operation of HVAC systems.

  • Read more

Combine energy measure and control, certified thermal energy measurement and billing

The Belimo Energy Valve™ integrates energy metering, control, delta T management, and if required IoT-enabled billing in one device. It offers seamless and direct integration to the BMS or to IoT-based monitoring platforms, with IoT-based monitoring, performance improvement tools, and billing data. The two worlds of "energy control" and "certified thermal energy measurement and billing" are being united. Bringing together performance features to save you time and money.

Energy measurement and power control anywhere

Access to the building data from anywhere and the transparency of the ventilation and heating systems are essential for the Lenzerheide Bergbahnen situated in the leading winter Alpine sports region and Switzerland's number one bike destination.

Energy saving you can see

The Belimo Energy Valve™ represents an easy to install, cost-effective option for resolving low delta T issues in district cooling systems. The successful implementation at the state-owned Citizen’s Plaza in Nashville (Tennessee, USA) perfectly illustrates the benefits of this solution.

Ensuring system reliability

Merck Biodevelopment, recently shared how the Belimo Energy Valve™ ensures system reliability in their manufacturing facilities in Martillac, France and enables them to achieve the right output, the right flow, and the right temperature at the right moment.

Energy billing with integrated energy meter

The University of Bremen campus has over 30 buildings built in the 1970s which have been repeatedly expanded and renovated. Increasing energy requirements over the years led to complicated volume distribution and maintenance of the cooling and heating supply. 
Thanks to the cooperation with Mr Florian Ruby from M&P Braunschweig GmbH and the installation of Belimo Energy Valves, the University of Bremen was able to solve the hydronic idiosyncrasies of this historically developed system. The power and mass flow rate control of the valves ensures a reliable supply. 
The generation systems will be optimally utilised and the individual buildings will be neither oversupplied nor undersupplied. 
The recorded data provide the University of Bremen's energy central with a high degree of transparency; a feat that was previously not possible with a basic control valve. 
Alongside the transparent monitoring and control of the heating and cooling system, the Energy Valve also allows for IoT-based, MID-approved energy billing within the individual cost centres.
 

  • Learn more about Belimo Energy Valves™

Products for better indoor air quality

Ensuring the quality of indoor air requires a multipronged approach. Besides precise system design and regular maintenance, reliable products which can be seamlessly integrated into building management systems and IoT platform are essential. Belimo offers a complete and innovative range of HVAC control devices to maintain healthy indoor air quality without compromising energy efficiency.

Discover products for healthy indoor air quality:

  • Learn more about reliable solutions for maintaining indoor air quality

The 7 essentials of healthy indoor air

The relationship between the design, installation, operation and maintenance of your HVAC system is vital to improve indoor air quality. Belimo identified 7 essential factors for ensuring healthy indoor air in buildings. 
 

Learn how to improve indoor air quality:

  • Belimo's 7 essentials to healthy indoor air

Influence of indoor air quality on our health

IAQ is often overlooked, and indoor air is naturally assumed to be safe to breathe. With most of our time spent indoors, this can be a dangerous assumption, as air quality affects our concentration, productivity, comfort and, most importantly, our health. 
 

Discover how IAQ influences our health:

  • Healthy indoor air quality

Good air quality for greater performance

In rooms without ventilation, the concentration of CO2 increases, performance drops rapidly, we are unable to concentrate, feel tired, suffer from headaches and much more. 
 

Indoor air quality has impact on our performance:

  • Good air quality for greater performance

Belimo celebrates the production of the 100 millionth actuator

At the beginning of 2020, Belimo produced its 100 millionth actuator and in doing so reached another milestone in the company's history. Today, hundreds of thousands of buildings around the world incorporate Belimo actuators into their HVAC systems.

The Swiss based world market leader for field devices for controlling and regulating heating, ventilation and air-conditioning systems continues its growth course by reaching this milestone as well as the demand for innovative products that sustainably increase comfort, energy efficiency and safety in buildings.

  • Read more

Ultrasonic flow sensor with glycol measurement

Trusted flow measurement is essential in maximising HVAC system efficiency and ensuring occupant comfort. Belimo’s new flow sensor utilises ultrasonic transit-time technology to provide accurate and repeatable flow measurements of water and water/glycol mixtures without drift in any HVAC application.

  • Multi-point wet calibrated to ensure accuracy and repeatability.

  • Patented temperature and glycol compensation logic eliminates manual calibration.

  • ±2% accuracy of reading and ±0.5% repeatability ensure accurate and precise flow measurement.

  • Read more

Providing safety in the McMenamins Elks Temple in Tacoma, Washington

Constructed in 1915, the historic Elks Temple Building is located on Tacoma's (WA) well-known Broadway and is listed in the National Register of Historic Places. In 2012, the Elks Temple was acquired by the McMenamins; after more than four decades of being abandoned. The building renovation started in 2017 with an aim to restore and preserve it to the early 20th-century architectural design and character of the theatre adding a restaurant, bars, hotel rooms, event spaces, and a working brewery. To protect the assets of the historic building and ensure the safety of the people, Belimo’s fire damper and smoke control damper actuators were installed.

  • Read more

Technology that saves lives

Fire protection in buildings is based on three main pillars: structural, technical and organisational fire protection. Technical fire protection is more important than ever, especially in modern buildings with unusual designs, mixed use or increasing building complexity and size. Belimo addressed this topic very early on, especially with regard to technical fire protection. As far back as 1978 –  three years after its foundation – Belimo sold actuators that could be mounted on fire dampers. In the meantime, Belimo has become the world market leader in the motorisation of fire dampers and smoke control dampers with well-founded expertise and experience.

  • Read more

Safety actuators

Land O’Lakes is committed to making the world a better place with Belimo Energy Valves.

  • Read more

Room comfort

Pressure-independent zone control in the Hongqiao SunnyWorld Centre, Shanghai.

  • Read more

RetroFIT+

The most intelligent butterfly valve actuator provides reliable integration of chilled water and waterside economizer

  • Read more

More power less energy

Proven user-friendliness and reliability of the new PR Actuators by Kuhn Champignon AG.

  • Read more

Butterfly valve

The refitted HVAC system commissioned in the production plant of SwissCo Services in May 2017, enabled energy savings of 128,000 kWh measured between May and August 2017.

  • Read more

Energy efficiency

The new Logistikcenter 4 of Galliker Transport AG in Dagmersellen delivers unparalleled energy efficiency.

  • Read more

Welcome to Belimo {{js-currentCountryName}}

{{js-currentCountryText}}
Contact Us Privacy Policy Safety Notes General conditions of sales and delivery Change privacy settings Imprint
+90 532 438 32 24
Subscribe
BELIMO Türkiye Otomasyon A.Ş., Serifali Mh. Hendem Cad. No: 38 Kesir Plaza Kat: 4, 34775 Ümraniye / İstanbul (Türkiye)