2. חדשות

6-way EPIV Receives BTL

The 6-way zone valve is used for the control of one terminal unit in 4-pipe operation, usually a cooling or heating ceiling or an air-conditioning beam. As a result of its unique technology – just one valve, one actuator and one control sequence – it revolutionises the structure of these systems and replaces conventional solutions (four 2-way valves, four actuators and two control sequences).

  • BACnet International
  • Learn more