חימום או קירור מרכזי / מחליף חום פלטות

  1. בית
  2. Belimo Energy Valve™ ומוני אנרגיה תרמית
  3. HVAC Applications

מה זה מחליף חום פלטות?

מחליפי חום פלטות משממשים לעיתים קרובות כדי להפריד מעגלים ראשיים ומשניים במערכות HVAC. מעגלים אלו עשויים להיות עם תנאי לחץ סטטי או תווך שונים. הספיקה עשויה להיות של זרם ישיר או של זרם נגדי.

מחליפי חום משמשים באופן נרחב במבנים גבוהים כדי להפחית את הלחץ הגרביטציוני שנוצר על ידי עמודי מים גדולים. מחליפי חום פלטות נפוצים גם במערכות חימום וקירור מרכזי. או במעגלי עומס לחימום מים חמים הראויים לשתייה באמצעות דוד.



Order the new Belimo Energy Valve™ now

Learn how the Energy Valve improves your plate heat exchanger





Energy Valve
Shop now




בעיות נפוצות במבנים ומדוע עליכם לבחור ב-Belimo Energy Valve™

Sometimes flow directions through the heat exchangers have not been chosen correctly. As a consequence the heat transfer capacity is reduced.

Heat Exchanger: Cooling transfer with direct flow    Heat Exchanger: ∆ϑm average temperature difference direct flow
The two figures below show two possible flow installations while the contraflow setup shows much better heat transfer. It results in larger delta T and thus higher energy efficiency to connect flow directions. The Energy Valve is able to recognize false flow directions. If this is detected an alarm flag will be sent to the BMS and this can be discovered during commissioning.

Heat Exchanger: Cooling transfer station contraflow    Heat Exchanger: ∆ϑm average temperature difference contraflow


A traditional setup plate heat exchanger will have an energy meter and a traditional balancing valve controlling the maximum flow through the heat exchanger. However, pressure fluctuations on the primary side cause the heat exchanger to overflow resulting in low delta T and poor heat exchange performance.

Heat Exchanger: Typical design flow (cooling application)    Heat Exchanger: ∆ϑm average temperature difference with design flow

Heat Exchanger: Overflow caused by pressure fluctuations    Heat Exchanger: ∆ϑm average temperature difference with overflow
By replacing the traditional balancing and control valve with a pressure independent valve, we solve the problem with the pressure fluctuations across the system. This is a step forward but still requires the application of multiple devices, including a separate thermal energy meter.

Heat Exchanger: Dynamic balancing
With a single EV we dynamically balance the system, monitor the energy usage for billing and record the delta T achieved. This reduces the equipment to be installed, making installation simple.

Dynamic balancing with delta T monitoring


Most Heat Exchangers suffer from fouling on one or both sides of the circuits. Minor fouling on one side can substantially affect the thermal energy transmission and drastically reduce the delta T.
The amount of time the Delta T Manager is active is indicative of the fouling process. If after a period of time the Delta T Manager remains active for extended periods then the heat exchanger should be cleaned or replaced.

סיפור הצלחה: בניין משרדים במדינת טנסי

בניין Citizens Plaza ניצב בלב העיר התחתית של נשוויל. בניין המשרדים מדרגה A, בשטח 25,550 מ"ר ועם 15 קומות נבנה בשנת 1984 והוא מאכלס מספר סוכניות ממשלתיות של מדינת טנסי. במהלך יום עבודה אופייני, נמצאים בו בין 800 ל-1,200 דיירים. "ב-Citizens Plaza, חווינו פליטות תרמיות חזקות מהתקנים שונים עקב חוסר יעילת שהגיעו ממערכת האנרגיה של הרכבת התחתית במחוז נשוויל, זאת בשל הפרש טמפרטורות נמוך ושאיבת יתר", סיפר צ'אד לובל, מומחה אופרציות ובטיחות ב- JLL. בסופו של דבר, הופעלו במבנה 15 ברזי אנרגיה של Belimio, כשהספיקה הממוצעת במבנה בזמן אכלוס מלא הופכת בכ- 200 GPM ‏(12.6 ליטרים/שנייה] לעומת השנה הקודמת כשסתומי הגלובוס המקוריים עדיין היו מותקנים. כתוצאה מפרוייקט ההתאמה לאחור, ברזי הארנגיה של Belimo הצליחו להפחית את שאיבת המים המקוררים ב- 49%, שווה ערך לכ- 23,000 דולר של חסכון שנתי.

  • Project Overview Video
  • Success Story - Tennessee State Building, USA (pdf - 1.91 MB)

Order the Belimo Energy Valve™ in our Webshop

  • Buy now

עוד על Belimo Energy Valve™

  • למידע נוסף

Belimo Energy Valve™ ביישומי HVAC אחרים

  • קרא עוד