RetroFIT+: Replacing Aging Actuators for Better HVAC Control
Actuators are small devices with a big impact on HVAC performance. When they are working properly, they help dampers and control valves respond to the control sequence and maintain airflow, ventilation, economizer operation, and overall system performance. When they age or fail, the symptoms can show up as comfort complaints, poor ventilation, unnecessary energy use, or hours of troubleshooting.
That makes actuator replacement a practical retrofit opportunity that can deliver meaningful improvements without requiring a full system overhaul. Building owners and facility teams can take a proactive approach, replacing aging actuators before total failure to restore more reliable control, improve visibility through the BMS, and modernize older pneumatic or outdated electronic devices.
Signs of Aging Equipment
Aging actuators in an HVAC system do not typically fail all at once. In many cases, they gradually lose performance. A damper or control valve may move slowly, fail to reach its commanded position, drift, hunt, or respond inconsistently. Linkages may loosen, gears may wear, housings may crack, and spring return functions may become unreliable. In pneumatic systems, leaks, cracked tubing, poor air pressure, and calibration issues can also affect performance.
These problems are often mistaken for larger system issues. For example, a failed economizer actuator can look like a cooling problem. A damper that does not open fully can affect ventilation or pressurization. On the waterside, a valve that does not respond correctly can affect coil performance, flow control, or temperature stability. A failed feedback signal can leave operators unsure whether the field device actually responded to the command from the control system.
Before replacing the actuator, the damper or valve assembly should be inspected. If blades are stuck, linkages are damaged, or the damper is binding, a new actuator will not solve the underlying mechanical problem. Similarly, if a control valve is seized, leaking, or improperly sized, replacing the actuator alone will not resolve the issue.
Moving from Pneumatic to Electronic Actuation
Many older buildings still have pneumatic actuators in service. They often depend on compressed air infrastructure, tubing, calibration, and maintenance of multiple components. Over time, leaks and drift can make control less consistent.
Electronic actuators can simplify the system and improve consistency. Belimo damper actuators are used in a wide range of airside HVAC applications, including air handlers, economizers, VAV terminal units, fan shutters, unit ventilators, and other damper applications.
Electronic actuators are also widely used in control valve assemblies in hydronic systems, including air handlers and fan coil coils, where accurate flow control is critical. Depending on the application, the retrofit may require a non fail-safe actuator, fail-safe actuator, outdoor protected actuator, quick running actuator, linear actuator, fire and smoke actuator, or an airflow measurement and control actuator.
The key is matching the actuator to the job. A basic control damper may need a different solution than an outdoor air damper, while applications such as economizer control, fire and smoke dampers, and airflow measurement and control systems require more specialized solutions.
Benefits of BMS Integration
Actuator replacement can also improve what the BMS can see. In older systems, the BMS may send a command without knowing whether the actuator actually reached the required position. Modern actuators with feedback or digital communication can reduce that blind spot.
Belimo actuators include options for analog control, feedback, field configurability, and digital communication such as BACnet, Modbus, or MP-Bus on select models. In some airflow measurement and control applications, actuators can communicate directly with the BMS and support pressure independent airflow control with integrated sensing.
For building operators, that visibility can make troubleshooting faster. Instead of assuming that a damper opened, the system can help verify position, identify faults, and confirm whether the actuator is following the sequence.
Sizing and Selection
A successful actuator retrofit depends on proper sizing and selection. The replacement should not be chosen only because it looks similar to the old actuator. The selection should account for torque, damper type, shaft size, control signal, supply voltage, running time, fail-safe requirements, rotation direction, mounting space, environmental conditions, feedback needs, and communication requirements.
Belimo SelectPro helps streamline this step by supporting sizing and selection for actuators and other HVAC field devices. For retrofit work, this gives contractors and facility teams a more structured way to narrow the options and choose the right actuator for the application.
Belimo offers a comprehensive range of actuator solutions. Non fail-safe actuators are suited for many standard HVAC damper applications. Fail-safe actuators are used where the damper must return to a defined position upon loss of power. Outdoor protected actuators provide NEMA-rated protection for exposed applications. Quick running actuators support faster damper movement where the sequence requires it. Linear actuators serve push-pull or linear motion applications. Airflow measurement and control actuators combine actuation with airflow sensing and control. Fire and smoke actuators serve life safety damper applications.
Fire and Smoke Replacement
Fire and smoke damper actuator replacement deserves separate attention because it is tied to life safety. These applications should not be treated like standard comfort-control dampers. Replacement selection must consider the damper assembly, torque, voltage, timing, temperature rating, fail-safe operation, required testing, and any listing or code requirements that apply to the specific fire and smoke damper application.
Belimo fire and smoke actuator solutions are designed for smoke and combination fire and smoke dampers in ventilation and air-conditioning systems. Select solutions also support remote testing and verification, allowing operators to initiate and confirm damper operation without physical access to the device.
Conclusion
Replacing aging actuators is a focused retrofit with a direct impact on HVAC control. It can improve damper response, reduce maintenance issues, support better BMS visibility, and help transition older pneumatic systems to more modern electronic control.
Whether the application calls for a non fail-safe, fail-safe, outdoor protected, quick running, linear, airflow measurement and control, or fire and smoke actuator, the goal is the same: restore reliable movement at the point where the control sequence meets the mechanical system. With the right selection process, supported by tools like Belimo SelectPro, actuator replacement can help buildings achieve better comfort, ventilation, reliability, and long-term serviceability.
Are you looking for HVAC training? Belimo offers unlimited access to a library of high-quality, current, and engaging HVAC video tutorials from industry experts. Participants report that Belimo training provides them with knowledge and skills that sharpen HVAC expertise.