Obiettivi ambientali

  1. Home
  2. Sostenibilità

Edifici e processi ad alta efficienza energetica

Belimo has made it its mission to create healthier, and more comfortable indoor environments that reduce energy consumption. In 2024, Belimo has committed to achieving net-zero greenhouse gas (GHG) emissions at the latest by 2050 with near- and long-term reduction targets aligned with SBTi Net Zero Standard. 

Belimo has developed a Group-wide methodology for GHG accounting. From the 2024 financial year, this balance sheet will be updated and disclosed annually as part of the external annual report. The Belimo GHG balance provides a comprehensive picture of all emissions (scope 1 to 3) caused by company activities over the course of a financial year. This includes:

  • The supply chain (procurement, upstream, intercompany, and downstream transport).
  • Assembly activities at all Production/Logistics and Customisation locations.
  • The use phase of devices in the field.
  • Device end-of-life treatment.
  • Business travel, company vehicles, and employee commuting.

Belimo decided to commit to the Science Based Targets initiative (SBTi) in 2024. This commitment is an important step towards climate change mitigation and ensures compliance with international regulations while also meeting stakeholder expectations.

  • Belimo aims to push the HVAC industry towards Net-Zero and is committed to the Net-Zero Target by 2050 outlined in the SBTi (Science-Based Targets initiative).

The challenge of achieving this ambitious goal is substantial and requires all stakeholders to contribute actively towards it.

With the help of the SBTi's internationally recognized and scientifically grounded approach for setting greenhouse gas reduction targets, companies can define a reduction path that is both ambitious and achievable, reducing greenhouse gas emissions both in their industry and along the value chain, and thus contributing to society's net-zero target.

  • Find Out More in the Press Release
  • Belimo GHG Accounting Methodology Emissions Calculation (PDF)

L'impegno per gli edifici sostenibili

Un esempio di trasparenza ed efficienza energetica

Per ottimizzare il sistema HVAC della sede centrale di Belimo siamo andati ben oltre, con un impianto di raffreddamento controllato e progettato in modo innovativo, che mette in mostra i nostri dispositivi di campo HVAC ad alta efficienza energetica e la trasparenza energetica che essi consentono.

Nel 2018 abbiamo iniziato la progettazione di un nuovo impianto di approvvigionamento di acqua refrigerata. L'obiettivo era quello di risolvere i difficili e persistenti problemi di comfort nell'edificio di produzione principale di Hinwil (Svizzera) e di sostituire l'impianto vecchio di 18 anni. Allo stesso tempo, abbiamo dato il via al passaggio a una nuova soluzione di building automation. 

  • Belimo Story: Future-Proof Chilled Water System (pdf - 1,03 MB)

Il progetto faro di Belimo in India

L'hub di Mumbai, la nostra sede indiana di 3,800 metri quadrati, è stato concepito per la prima volta nel 2016 come parte della nostra strategia di crescita accelerata per il 2030. L'edificio, costruito come vetrina di soluzioni HVAC all'avanguardia e di design sostenibile, ha rappresentato un'opportunità entusiasmante per progettare una struttura ecologica dalle fondamenta.

L'edificio comprende uffici e stabilimenti, tra cui un centro di assistenza clienti Belimo, creato per supportare attivamente il percorso dei clienti verso la creazione di un comfort interno più sano con meno energia. Inoltre, offre agli OEM e agli accademici un luogo in cui collaborare per progettare, costruire e testare la prossima generazione di prodotti Belimo.


Uno dei più grandi sistemi di generazione di energia solare in Connecticut, USA

L'impianto solare da 876 kW presso la sede di Belimo Americhe, che incorpora 2192 moduli solari ad alto rendimento, ha una produzione annua di circa un megawattora di elettricità. Utilizzato per compensare una parte del fabbisogno energetico di Belimo con l'energia solare, consentirà di risparmiare 857 tonnellate di emissioni di gas serra, equivalenti al fabbisogno annuale di circa 100 abitazioni nel Connecticut.

  • LEED Gold, Belimo Americas Expansion Project (Danbury/USA) (pdf - 1,42 MB)
  • LEED Gold, New Construction: Belimo Aircontrols (Sparks/USA) (pdf - 232 KB)

Creare un comfort ambiente più sano con meno energia

Gli edifici sono responsabili del 40% della domanda globale di energia e delle emissioni di gas serra. E poiché trascorriamo fino al 90% del nostro tempo in ambienti chiusi, essi hanno un forte impatto sul nostro comfort, sulla nostra salute e sul nostro benessere generale. La missione di Belimo è quella di creare ambienti interni più sani e confortevoli che consumino meno energia. Con un portafoglio di prodotti naturalmente orientato alla realizzazione di diversi Obiettivi di Sviluppo Sostenibile delle Nazioni Unite, realizziamo sistemi di building automation e di controllo degli edifici (BAC) ad alta efficienza energetica che riducono i requisiti energetici delle soluzioni HVAC fino al 55%.

  • Belimo è impegnata nella sostenibilità

Altri argomenti correlati

Contributi agli Obiettivi di Sviluppo Sostenibile (SDG)

  • Per saperne di più

Responsabilità sociale

  • Per saperne di più

Governance

  • Per saperne di più