Small Devices, Big Impact.
Innovations Redefining Comfort

  1. Faqja kryesore
  2. CESIM

Solutions For Comfort

State-of-the-art building automation is indispensable in generating good air quality and pleasant temperatures for best possible room climates. But ideal air quality is not the only pre-requisite for room comfort – the pressure ratios between supply- and return air must be maintained in rooms and air ducts. The ability to control individual room climates is all the more important. Reliable HVAC components from Belimo perfectly harmonize these influencing factors, so that ensured room comfort and productivity prevail at all times in different rooms.
Heating and cooling components in the central plant, air handling units, and terminal units for the room are fitted with sensors, damper actuators, and control valves and are networked with each other for the best sense of well-being in rooms. Our intelligent HVAC components deliver excellent air quality for the highest level of room comfort.

Our Sensors – The Foundation of Comfort

The Belimo sensor range is a result of over four decades of experience, research, and focus on providing value-adding technologies to customers throughout the HVAC industry. The sensors’ unique design offers easy installation and seamless integration, resulting in reduced costs and optimal system performance. We offer a complete range of sensors with high accuracy and long-term stability, resulting in better indoor comfort. Our broad product portfolio provides sensors for measuring temperature, humidity, pressure, CO2, volatile organic compounds (VOCs), and flow in pipe, duct, and outdoor applications. Belimo serves as your single-source provider of HVAC field-level devices for any building project.

  • Our Sensor Range

Learn More: The Key Factors Influencing Thermal Comfort

While there are guidelines for indoor air quality, the situation variables such as room function, clothing, activity level of those in the room, and simply the very personal needs of room occupants vary greatly. The temperature of the room becomes more noticeable the longer one is in it. During the heating period, temperatures that range from 20 to 22° C (compared to 25 to 26° C in summer) are recommended at floor level. Excessively high or low humidity also has a bearing on well- being, productivity, and even health. Learn more about the influencing factors of thermal comfort.

  • Presentation: Thermal Comfort is Influenced by Many Factors (pdf - 1,79 MB)
  • Our Sensor Range

Pressure Independent Control Valves for a Perfectly Balanced Room Comfort

Pressure Independent (PI) control valves ensure that hydronic systems are perfectly balanced at all times, leading to better comfort. The ball valve technology maximizes energy savings of variable flow pumping systems while addressing unique control challenges. Watch the Belimo Talk below and learn more about the dynamics of a hydronic system and how to ensure that the building performance matches the design size of the valves perfectly. Belimo offers a series of pressure independent (PI) control valves; from the PIQCV, a super compact PI valve, ePIV an electronic PI valve offering true flow measurement to the Energy Valve that optimizes, documents and proves water coil performance.

  • Pressure Independent Control Valves

Learn from Rodrigo: How to Provide Comfort with Pressure Independent Valves

Learn from Rodrigo: How to Achieve a Perfectly Balanced Hydronic System

Delivering the required flow in hydronic systems can be challenging with pressure changes. The Belimo Hydronic Simulator helps you understand the dynamics of a hydronic system with manual balancing and pressure independent valves. Download the Belimo Hydronic Simulator™ as an Excel file and learn how to use the Belimo Hydraunic SimulatorTM with the Belimo Talk taught by Rodrigo.

 

  • Belimo Hydronic Simulator (xlsm - 5,94 MB)

Energy Efficient Comfort

Smart Belimo devices provide optimal indoor air quality while increasing energy efficiency. Innovations that have a big impact on better room comfort.

  • Zip Economizer
  • Zip Economizer Video