2. Belimo Blog

Room Sensors Wins Innovation Award

Publié par
Lisa Hickey
le mer., nov. 09, 2022 @ 05:06 p.m.

Belimo Room Sensors recently won the AHR Innovation Award in the Indoor Air Quality category. The annual awards competition honors the most innovative and original products, systems, and technologies showcased at the International Air-Conditioning, Heating, Refrigerating Exposition (AHR Expo) in the categories of building automation; cooling; green building; heating, indoor air quality, plumbing; refrigeration; software; tools & instruments; and ventilation.

Belimo Room Sensors are essential for controlling and monitoring airflow to provide safe indoor air environments. A Red Dot award-winning design with an ePaper touch display provides high contrast and intuitive operation, illustrating current room values with the ability to adjust setpoints. The tri-color LEDs indicate the CO2 concentration levels at a glance. The CO2 measurements are automatically adjusted based on altitude, making these room sensors more accurate under varying conditions. 

 

Commercial applications are the best fit for Belimo Room Sensors. Businesses can reduce waste and operational costs by implementing energy-efficient measures, especially for spaces with variable occupancy. As a result, building managers can lower maintenance expenses and provide employees and customers with a comfortable working environment. The Room Sensors are maintenance-free and provide long-term reliability for a comfortable room environment. Integrated Near Field Communication (NFC) offers easy field adjustability, commissioning, remote display capabilities, and troubleshooting even without power. For devices without an integral ePaper display, setpoints can be programmed using the new Belimo Room Display App, which turns your smartphone into a remote display. Apps associated with Belimo's room sensors allow password protection capability for an added security layer and can disable NFC for applications requiring increased security.

 

Collège Laval maintains an unparalleled quality of education by taking the health of its students and staff very seriously. By installing 115 Belimo room sensors within the college, it is now possible to precisely detect air quality in real-time, even from a smartphone. To achieve this, the college staff worked with Immotik, a distributor, installer, and integrator of BACnet products, to select and install a network of sensors in the six wings of the college. Every sensor can be scanned quickly and easily to access data in real-time, without prior calibration, via the Belimo Assistant App and a smartphone. It also allows field adjustment, commissioning, and troubleshooting even without power.

 

  • ePaper Touch Display
  • CO2 Traffic Light
  • Configurable
  • Snap Cover
  • Removable Terminal
  • Quick Response Time
  • High Accuracy
  • Seamless Integration
  • NFC Capabilities
  • High contrast and intuitive operation illustrating current room valves with the ability to adjust setpoints
  • The LED shows the CO2 concentration (not visible in the off position).
  • Set the display to show only measured valves or temperature and fan setpoints.
  • The design allows for quick installation and easy commissioning.
  • Spring-loaded terminal block saves wiring time and ensures reliable contact.
  • The sophisticated technology allows the sensor to react very quickly to changes in temperature.
  • The low wall coupling factor provides accurate measurements unaffected by the wall temperature.
  • With BACnet, Modbus and MP-Bus can communicate directly to the BMS.
  • Parameterize and adjust the room sensor through the Belimo Assistant App
  • For non-ePaper display variants, the Belimo Room Sensor Display app brings display and setpoint capabilities to a smartphone.

PRODUCT SERIES
Temperature
Temperature with Setpoint Temperature + Relative Humidity
Temperature + Relative Humidity + CO2

Explore the product offering online.

 

Étiquettes : Belimo News, Green Building Technology, Product Updates, Sensors

Retour au blog

Articles connexes

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read En savoir plus

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read En savoir plus

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read En savoir plus