2. Belimo Blog

What is a Butterfly Valve?

Publié par
Jason Tables
le mar., juin 03, 2025 @ 04:23 p.m.

What is a Butterfly Valve?

If you work in HVAC or plumbing, you’ve likely come across butterfly valves. But what defines them, and how do they differ from other valve types? A butterfly valve is a flow control device that uses a rotating disc to regulate or isolate fluid movement. Butterfly valves can handle large volumes with less space and weight compared to other valve types, making them a favorite in HVAC applications where efficiency and compactness matter. The word “butterfly” refers to the metal disc that turns within the pipe to open or restrict flow. With a simple 90-degree turn, the valve shifts from fully open to fully closed.

Why would you use a butterfly valve?

Butterfly valves are widely used in systems that require reliable shut-off and flow regulation without the footprint or complexity of bulkier valve types. They’re especially useful in large-diameter piping where minimizing pressure drop and weight is critical. Their simple mechanism allows for fast actuation, and with the right actuator, they’re well-suited for on/off, 3-point, or modulating control. In HVAC, this makes them ideal for chilled water, hot water, and condenser water systems where space, efficiency, and installation time are all important factors.

Why use a butterfly valve instead of a ball valve?

While ball valves also offer quarter-turn actuation, butterfly valves are generally more compact and lighter—especially in larger sizes. Ball valves become bulky and expensive as diameter increases, whereas butterfly valves maintain a slim profile and cost-effectiveness. Additionally, butterfly valves can be configured for tight shut-off and modulating control in large HVAC systems, where ball valves are typically favored for smaller, more localized applications. When you’re dealing with flow control in 4" or larger pipe, butterfly valves tend to offer better overall value.

Why use a butterfly valve instead of a gate valve?

Gate valves are designed for full open or full closed service, but they’re slower to operate and tend to have more maintenance issues over time due to sediment buildup in the gate track. Butterfly valves, by contrast, actuate quickly with a simple 90-degree turn and take up less space, making them easier to install in tight mechanical rooms. They also tend to provide a better seal in modern systems and offer more flexible control options when paired with actuators. For applications requiring frequent operation or remote actuation, butterfly valves are generally the better choice.

Why use a butterfly valve instead of a globe valve?

Globe valves are known for their precise flow control, but that precision comes at the cost of pressure drop, size, and weight. In HVAC systems, particularly those with large pipe diameters, a globe valve can be prohibitively heavy and expensive. Butterfly valves offer a compelling alternative: with proper actuator pairing, they can deliver equal percentage or linear flow control while minimizing pressure losses and taking up far less space. That’s one reason Belimo butterfly valves, in particular, are replacing globe valves in many high-performance systems.

What makes Belimo butterfly valves different?

Belimo’s advanced butterfly valve assemblies are specifically engineered for HVAC systems, offering a combination of smart design, high energy efficiency, and proven long-term reliability. They feature a patent-pending, self-adjusting end stop algorithm that delivers zero leakage at up to 200 psi close-off. The actuators use our patented brushless DC motor technology to reduce energy consumption by up to 80%, while the integrated high-performance processor enables precise flow control. Our compact actuator design allows for installation in tight spaces, and NFC functionality allows for fast commissioning, programming, and diagnostics, even without power. With proven performance across large flow applications and a five-year warranty, Belimo butterfly valves offer a durable, efficient solution for demanding HVAC systems.

How do Belimo valves help save energy?

This is one of the most common questions asked when people are considering an upgrade. The short answer is smart torque management. Belimo matches each butterfly valve with an actuator that is designed to deliver only the exact torque required. This reduces wasted energy, extends actuator life, and ensures consistent performance over time. Combined with low pressure drop and efficient design, Belimo butterfly valves make a meaningful contribution to overall energy savings across the system.

Are Belimo butterfly valves easy to install?

Ease of installation matters, especially when you're working in tight mechanical rooms or upgrading legacy systems. Belimo butterfly valves are much lighter and shorter than traditional globe valves. A 3-way 8-inch Belimo butterfly valve, for example, weighs less than half of what a similar-sized globe valve weighs and is half the height. That reduction in size and weight not only makes installation faster, it also places less physical strain on the piping system.

Can Belimo valves connect to building automation systems?

Yes. Belimo butterfly valves are designed for full compatibility with building automation systems through support for BACnet MS/TP, Modbus RTU, and Belimo’s MP-Bus protocols. The PR, PKR, and JR actuator series all include these communication capabilities, allowing seamless integration with most building management platforms. Each actuator series also features Near Field Communication (NFC), which enables quick programming, diagnostics, and commissioning without the need for power. This combination of connectivity and serviceability makes it easier to monitor, configure, and optimize valve performance directly from a centralized system.

Are Belimo valves compatible with sensors?

Definitely. Belimo actuators support direct sensor inputs, which means you can wire sensors right into the actuator without needing to run them all the way back to the controller. This not only simplifies installation but also lowers costs by reducing wiring and setup time. It’s a design choice that supports smarter building designs and faster installations.

Are Belimo valves reliable in tough environments?

Durability is a big concern, especially in rooftop installations or damp mechanical spaces. Belimo butterfly actuators are built to NEMA 4X standards, meaning they can withstand dust, rain, and other challenging conditions. The valve bodies are ductile iron, and the internal discs are stainless steel, ensuring strength and corrosion resistance. These aren’t throwaway components. They’re built for the long haul.

Can Belimo butterfly valves provide precise control?

Yes, and that surprises a lot of people. These valves are not just on/off devices; they’re capable of both equal percentage and linear flow characteristics. That gives you the precision needed for variable flow applications and ensures your system responds smoothly to demand. With the Belimo Assistant 2 App, you can customize settings right from your phone, including adjusting CV values or modifying control curves.

Are Belimo butterfly valves worth it?

When you consider the full picture, including tight shut-off, energy savings, flexible installation, smart integration, and long-term reliability, it’s hard to argue against them. Belimo’s butterfly valves are a strong fit for HVAC pros looking for a future-ready system that avoids constant maintenance and complicated setup.

Are you looking for HVAC training? Belimo offers unlimited access to a library of high-quality, current, and engaging HVAC video tutorials from industry experts. 

Étiquettes : Butterfly Valves

Retour au blog

Articles connexes

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read En savoir plus

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read En savoir plus

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read En savoir plus