Retrofitting Pressure Dependent HVAC Systems to Pressure Independent Control
How do you retrofit a pressure dependent HVAC system?
A pressure dependent HVAC system is typically retrofitted to pressure independent control by upgrading the field devices that regulate flow through the heating and cooling coils. In practice, that usually means replacing pressure dependent valves with pressure independent control valves that maintain the required design flow by compensating for differential pressure changes across the system
For many existing buildings, this kind of retrofit is a practical way to improve hydronic performance without replacing the entire HVAC system. Legacy pressure dependent systems may have performed exactly as designed on day one, but building conditions rarely remain unchanged. Tenant spaces are renovated. Occupancy patterns shift. Equipment ages. Control sequences are adjusted. Over time, those changes make a system harder to balance, harder to troubleshoot, and less efficient to run.
When pressure dependent systems begin to drift, the symptoms are familiar to most facility teams: unstable flow, low Delta T, comfort complaints, over-pumping, and little visibility into what is actually happening at the coil. The system keeps running, but it is no longer delivering the control or efficiency the building needs.
Why pressure dependent systems become harder to manage
Pressure dependent system performance relies heavily on stable pressure conditions and manual balancing. In a real building, this is a fragile assumption, because loads and operating conditions change throughout the day. An adjustment in one part of the circuit shifts the differential pressure for all the other coils on the same loop.
When pressure shifts, a traditional pressure dependent valve can pass too much or too little water through the coil. Too much flow drives low Delta T and wastes pumping energy; too little starves the coil and undercuts comfort.
Pressure independent control maintains the set flow within the valve’s operating differential pressure range, even as system pressure changes. Belimo pressure independent control valves are built for variable-flow pumping systems and can be configured to the required design flow (GPM) for each circuit, so the system performs to the design spec without manual balancing.
For buildings that need deeper visibility, the Belimo Energy Valve™ goes further by adding integrated flow, temperature, and energy measurement to pressure independent valve control, supporting Power Control, Delta T Manager logic, and cloud-connected analytics. Together they turn the coil itself into a measurement point, so operators can judge coil performance and uncover problems that would otherwise stay hidden.
How coil-level data improves troubleshooting
Beyond flow control, the value of electronic pressure independent solutions is increased visibility into coil performance. In a legacy system, a valve can be open, a pump can be running, and a space can still be uncomfortable. Without measured flow, temperature, and energy data, it is hard to tell whether the issue is at the coil, the valve, the pump, the control sequence, or somewhere else in the system.
With coil-level data, facility teams can compare actual flow, temperature, and energy performance against the control sequence to see whether the system is delivering the intended flow and heat transfer, or whether the valve, coil, pump, or sequence needs attention. This measured data can also support ongoing commissioning, fault detection, and performance verification.
Real-world retrofit results
At Four Embarcadero Center in San Francisco, a 48-story tower owned by BXP, the 40-year-old chilled water system still relied on two-way, pressure dependent globe valves with pneumatic actuators, and the result was chronic low Delta T, rising energy costs, and no visibility into hydronic performance. BXP retrofitted all six air-handling units with Belimo Energy Valves, converting the system to pressure independent operation and providing real-time flow, temperature, and energy measurement at each coil. This measured data showed that low Delta Ts of 1–3°F were being caused by a bypass valve that was stuck open and bleeding chilled water through the system. After the issue was corrected, summer Delta T rose to more than 14°F, chilled water use dropped by roughly half, and chiller plant energy consumption fell 28%, saving about $131,000.
In New York City, Paramount Group upgraded three premier commercial properties with Belimo Energy Valves to meet Local Law 97, the city’s mandate to cut building carbon emissions beginning in 2024. The legacy two-way pneumatic valves offered little controllability, and 18°F design coils were running closer to a 5°F Delta T. The retrofit established pressure independent control across the buildings and brought the coils back to their design 18°F, and above 20°F in places, restoring both coil performance and the Delta T the system was built for.
The project also shows how incentives strengthen the financial case. Across 2023 the three buildings cut more than $1 million in utility costs, and because the Energy Valves logged exportable kWh and BTU data, that performance was easy to prove to the utility, work that secured a further $2.1 million in rebates.
When should a building consider a pressure independent retrofit?
A building is often a strong candidate for a pressure dependent to pressure independent retrofit when it shows recurring balancing problems, low Delta T, comfort complaints, unstable flow, aging pneumatic valves, excessive pumping energy, or limited visibility into coil performance. These symptoms cluster in many older commercial buildings, where HVAC systems have been modified piecemeal over the years and balancing efforts often deliver diminishing returns.
A pressure independent retrofit rarely requires a full mechanical redesign. More often, targeted field-device upgrades are enough to improve control, restore performance, and reveal system data. RetroFIT+ supports these projects with replacement solutions for existing valves, actuators, sensors, and related components. The RetroFIT+ App for iOS and Android, and the Belimo RetroFIT+ Product Replacement Tool for desktop help match obsolete or defective field devices with suitable Belimo replacements, making it easier to plan and execute targeted upgrades.
For owners and facility teams, a pressure independent retrofit delivers a clear value proposition: stable flow control, improved energy efficiency, measurable system performance, and a practical path to modernizing existing hydronic systems. Utility incentives can further strengthen the return, though eligibility and program availability vary by utility and region.
Are you looking for HVAC training? Belimo offers unlimited access to a library of high-quality, current, and engaging HVAC video tutorials from industry experts. Participants report that Belimo training provides them with knowledge and skills that sharpen HVAC expertise.