2. Belimo Blog

Belimo at the 2025 AHR Expo

Publié par
Jason Tables
le jeu., févr. 13, 2025 @ 05:41 p.m.

The 2025 AHR Expo took place in Orlando, Florida, from February 10 to 12, attracting a diverse range of professionals and exhibitors from across the HVACR industry. Belimo's booth was a focal point for many attendees, showcasing a variety of innovative HVAC solutions. Attendees were particularly interested in the Belimo Advanced Butterfly Valve featuring the new JR actuator, which offers outstanding reliability and advanced features specifically tailored for smaller valve sizes.

The booth also featured Belimo’s award-winning Room Sensors and the Energy Valve, an IoT-enabled device that combines energy monitoring, precise flow control, and Delta T management. Additionally, the newly released Belimo Assistant 2 app was highlighted as an all-in-one tool for managing the entire lifecycle of Belimo devices.

In addition to the booth activities, Product Specialist Steve Lopes delivered a presentation in the New Product Technology Theater, showcasing the Belimo Advanced Butterfly Valve with the new JR actuator. Steve’s insights provided attendees with a deeper understanding of the product's new features and improvements, which include a streamlined installation process as well as an 80% reduction in energy consumption.

The 2025 AHR Expo was a resounding success, leaving attendees with valuable insights on Belimo’s innovative products and solutions. A standout moment was a toast led by Belimo CEO Lars van der Haegen and Belimo Americas President James Furlong celebrating Belimo's 50th anniversary, with customers and associates joining for champagne and refreshments.

Étiquettes : Damper Actuators, Butterfly Valves, Energy Valve, Gas Monitors, Electronic Pressure Independent Valves (EPIVs), Sensors

Retour au blog

Articles connexes

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read En savoir plus

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read En savoir plus

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read En savoir plus