2. Belimo Blog

How Control Valves and Hydronic Systems Interact

Publié par
Lisa Hickey
le mar., févr. 23, 2021 @ 03:00 p.m.

Motorized valves control and adjust water flow in a hydronic heating and cooling system. The flow through pressure dependent valves varies as the pressure (∆P) across the valve orifice changes. Typical pressure dependent valves include globe valves, zone valves, characterized control valves,  standard ball valves, and butterfly valves. When pressure varies in a system, the flow will have an identical response. As the pressure drop decreases across a pressure dependent control valve, flow decreases, starving the coil or branch. When pressure drop increases across a pressure dependent control valve, flow increases, flooding the coil or branch. Overflowing the coil usually causes what we call low Delta T syndrome. This syndrome typically increases the energy consumption of chilled water pumps, decreases system overall operating efficiency, undermines occupant comfort, and increases overall operation cost. 

With a pressure independent (PI) valve, one valve replaces two valves. A pressure independent (PI) valve combines a dynamic balancing valve and control valve to supply accurate and stable flow while maintaining a balanced system even when flow fluctuates as demand changes. When a standard control valve (pressure dependent) is oversized at average to light loads (95-99% of operation time), it may oscillate or hunt. The pressure independent valve has an equal percentage response curve under all conditions, which results in a linearized power output to the control signal. A pressure independent valve provides consistent flow for each degree of ball opening with no adjustments required. To maintain dynamic balancing, a PI valve needs a minimum of 5 psi pressure drop. The minimum differential pressure is significantly less than a pressure dependent control valve and circuit setter/balancing valve combined. PI values enable you to lower pump head pressure and reduce the high cost associated with over-pumping. With a pressure independent valve pressure variations are no longer a concern; the valve act with an inherent characteristic valve authority. Direct return systems can utilize pressure independent valves to achieve self-balancing behavior and eliminate costly reverse return piping.

 

Sizing a pressure dependent valve cannot be accurate without a firm understanding of the hydronic system. While valves are the final control element, balancing, coil sizing, coil response curve, and piping losses all play a role in accurate sizing. A control valve cannot be adequately sized without a full analysis of the system. All components interacts in a hydronic system, so the valves cannot be treated as a simple subject by themselves. Instead, the whole hydronic system has to be taken into account.

There is a good deal of data required for careful sizing and selecting valves, but when all of it is not available, the accuracy will suffer. The specifications do not always take as-built conditions into account and valves may be incorrectly sized. In such situations, the design engineer should be consulted. Every process, every coil has a unique response. It isn't easy to design a valve for every control process.

For more information and recommendations, please contact your local Belimo support.

Étiquettes : Green Building Technology, Electronic Pressure Independent Valves (EPIVs)

Retour au blog

Articles connexes

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read En savoir plus

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read En savoir plus

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read En savoir plus