2. Belimo Blog

Smart Self-Balancing Bypass Damper Receives Silver Award

Published by
Lisa Hickey
on Tue, Jan 05, 2021 @ 11:03 PM

EWC Controls receives the Silver Award in the ACHR News Magazine Dealer Design Awards for its Smart Self-Balancing Bypass Damper - SBD2. Available in round and rectangular dimensions, the SBD2 serves to bypass "only enough" airflow to restore proper static pressure to an HVAC system during zoned operation.

EWC is an industry leader in zoning solutions for residential and light commercial applications. They are a third-generation family-run business that has found immense success through close collaboration with customers, enabling product developments that exceed expectations. The original SBD was born out of this collaborative process and was quickly recognized for revolutionizing bypass damper technology by winning a 2016 Dealer Design Award. Since then, thousands of zoned HVAC systems across the country benefit from its state-of-the-art bypass control. The second-generation SBD2 incorporates NFC (Near Field Communication) to provide contractors with wireless access to the smart actuator with a free Android or iOS Assistant App.

The primary feature of the SBD2 product is its quick and easy setup. Just press a button, and the actuator will learn the ideal system static pressure and apply the appropriate pressure setpoint. With NFC's introduction, the installer can now manually set the desired pressure or tweak the setpoint learned during the automated process. With SBD2, you get easy setup plus complete flexibility in the same product.

HVAC technicians, while using the app, can also see live charts of real-time data, including damper position, static pressure, and desired static pressure. EWC recognized that some contractors might not have a manometer close at hand, but they all have smartphones. The app can act as a "digital" manometer that is always handy. Charts of live data can be saved with personalized name and location details and then emailed directly from a smartphone. The app is invaluable for customer verification or remote recordkeeping and support.  

Belimo is exceptionally proud of the SBD’s success. With the NFC upgraded SBD2, they have leveraged enhancements to Belimo’s smart actuator platform to embed customer "know-how" into a powerful yet easy to use product that solves problems while saving time and money.

Download the SBD2 datasheet from the EWC website. Specify the award-winning smart self-balancing bypass damper with NFC on your next HVAC zoning project.

Tags: Belimo News

Back to Blog

Related Articles

Online Learning Resources & Tools, Technical Tips

What is CV, and How Do I Calculate It?

Valve Flow Coefficient (Cv) is defined as the volume of water at 60°F that will flow through a fully open...

1 minute read Read More

Technical Tips

Importance of Dampers and Actuators in HVAC Systems

Dampers are the final control devices for almost all airflow in HVAC systems. Actuators are the interface between the control system.

2 minute read Read More

Sensors, Technical Tips

Understanding HVAC Sensors

Some of the most critical sensors used in HVAC systems are pressure, temperature, humidity, air quality, occupancy, and room sensors.

1 minute read Read More