• Building owners
    • HVAC professionals
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
    • Building owners
    • HVAC professionals
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
District Heating or Cooling / Plate Heat Exchanger

  1. Home
  2. Belimo Energy Valve™ and Thermal Energy Meter
  3. HVAC Applications

What is a Plate Heat Exchanger?

Plate Heat Exchangers are often used to separate primary and secondary circuits in HVAC systems. Those circuits may have different medium or static pressure conditions. Flow can be direct current or counter current.

Heat exchangers are extensively deployed in tall buildings to reduce the gravitational pressures provided by large water columns. Plate heat exchangers are also very common in District Heating and Cooling systems. Or in load circuits to heat potable hot water with a boiler.



Order the new Belimo Energy Valve™ now

Learn how the Energy Valve improves your plate heat exchanger





Energy Valve
Shop now




Common Issues in Buildings and Why You Should Choose the Belimo Energy Valve™

Sometimes flow directions through the heat exchangers have not been chosen correctly. As a consequence the heat transfer capacity is reduced.

Heat Exchanger: Cooling transfer with direct flow    Heat Exchanger: ∆ϑm average temperature difference direct flow
The two figures below show two possible flow installations while the contraflow setup shows much better heat transfer. It results in larger delta T and thus higher energy efficiency to connect flow directions. The Energy Valve is able to recognize false flow directions. If this is detected an alarm flag will be sent to the BMS and this can be discovered during commissioning.

Heat Exchanger: Cooling transfer station contraflow    Heat Exchanger: ∆ϑm average temperature difference contraflow


A traditional setup plate heat exchanger will have an energy meter and a traditional balancing valve controlling the maximum flow through the heat exchanger. However, pressure fluctuations on the primary side cause the heat exchanger to overflow resulting in low delta T and poor heat exchange performance.

Heat Exchanger: Typical design flow (cooling application)    Heat Exchanger: ∆ϑm average temperature difference with design flow

Heat Exchanger: Overflow caused by pressure fluctuations    Heat Exchanger: ∆ϑm average temperature difference with overflow
By replacing the traditional balancing and control valve with a pressure independent valve, we solve the problem with the pressure fluctuations across the system. This is a step forward but still requires the application of multiple devices, including a separate thermal energy meter.

Heat Exchanger: Dynamic balancing
With a single EV we dynamically balance the system, monitor the energy usage for billing and record the delta T achieved. This reduces the equipment to be installed, making installation simple.

Dynamic balancing with delta T monitoring


Most Heat Exchangers suffer from fouling on one or both sides of the circuits. Minor fouling on one side can substantially affect the thermal energy transmission and drastically reduce the delta T.
The amount of time the Delta T Manager is active is indicative of the fouling process. If after a period of time the Delta T Manager remains active for extended periods then the heat exchanger should be cleaned or replaced.

Success Story: Tennessee State Office Building

Citizens Plaza stands in the heart of Downtown Nashville. The Class A, 275,000 square feet,15-story office building was constructed in 1984 and houses multiple Tennessee governmental agencies. During a typical workday, it has anywhere from 800 to 1,200 occupants.“At Citizens Plaza, we were experiencing high utility thermal inefficiency charges from Metro Nashville District Energy System due to low Delta T and over pumping,” said Chad Lovell, Operations and Safety Specialist at JLL. After all, 15 Belimo Energy Valves became operational in Citizens Plaza, the average flow through the building during full occupancy reduced by over 200 GPM [12.6 l/s] versus the previous year when the original globe valves were still in place. As a result of the retrofit project, Belimo Energy Valves were able to reduce chilled water pumping by 49%, which equated to about $23,000 in annual savings.

  • Project Overview Video
  • Success Story - Tennessee State Building, USA (pdf - 1.91 MB)

Order the Belimo Energy Valve™ in our Webshop

  • Buy now

More about the Belimo Energy Valve™

  • More information

The Belimo Energy Valve™ in other HVAC Applications

  • Read more

Welcome to Belimo {{js-currentCountryName}}

{{js-currentCountryText}}
Contact Us Privacy Policy Change privacy settings Safety Notes Imprint
+2 0100 677 06 06
Subscribe to newsletter
BELIMO Egypt, 3 Omar Ibn Abd El Aziz Street, First 6th of October, Giza Governorate 3234126 (Egypt)