• Building owners
    • HVAC professionals
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
    • Building owners
    • HVAC professionals
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
Training

As a market-leading company, we are committed to sharing our knowledge and innovative edge with you in the simplest possible way. In addition to our numerous webinars, which you can find under the heading Webinars, we offer educational videos and web-based trainings on a wide range of exciting topics.
Online training gives you access to further education from anywhere and anytime. In the diversified self-study courses, you can acquire the information we provide on our products and general applications.

Is there a topic you would like to be informed about? Let us know! 

  • Educational videos
  • Web-based training
Educational videos

In this section we offer extensive knowledge transfer through short video sequences.

Smart control strategies for maximum energy efficiency (in German)

Duration: 28 minutes

Time and again, buildings are found to have an improvable energy balance. Depending on the year of construction and the sometimes incomplete technical documentation available, a considerable potential for savings exists. This can result in an uneven distribution of heat and cold in the building, which increases maintenance and energy costs. With pressure-independent control valves and smart sensor technology, the building technology can be controlled precisely and as required. This increases energy efficiency and reduces maintenance costs.

In this learning video, speaker Bernd Wittenberg, strategic consultant at Belimo, will discuss the possibilities of intelligent control strategies for the efficient air-conditioning of buildings.

  • Watch the educational video here

Control condensation with the new pressure-independent 6-way valve from Belimo (in German)

Duration: 22 minutes

This educational video shows the innovative solutions that Belimo offers with its new pressure-independent 6-way valves, as well as how to prevent condensation before it occurs.

In addition to the standard 6-way EPIV, two variants featuring condensation management were launched: 

  • 6-way EPIV with condensation switch: detects condensation 
  • 6-way EPIV with humidity sensor: measures relative humidity and acts as an "early warning system" 

The new pressure-independent 6-way valves from Belimo continue to offer the proven technology that combines flow measurement and a characterised control valve, now also with condensation monitoring in one device.

  • Watch the educational video here

Typical problems with valve design in 3-way mixing circuits — and how to avoid them (in German)

Duration: 37 minutes

In practice, specialist planners and installers often encounter 3-way mixing circuits. These circuits are popular because they enable simple flow temperature control. However, especially when integrating modern heat generators such as district heating or heat pumps, the “standard” dimensioning of the valves can lead to design errors. 

The problem: lack of control stability due to incorrect dimensioning.
The solution: harmonise the hydronics and valve in a targeted manner

  • Watch the educational video here

Efficient cooling for future-proof data centres (in German)

Duration: 31 minutes

Efficient cooling is the backbone of high-performance data centres. However, with increasing power densities, the advent of AI applications, and high-performance computing (HPC), as well as stricter regulatory requirements, classic air cooling systems are increasingly reaching their limits. Operators are, therefore, faced with the challenge of developing innovative and sustainable cooling strategies without compromising availability or energy efficiency.

In our instructional video, we show you how you can use intelligent components and pioneering cooling strategies to make your infrastructure fit for the demands of tomorrow. At the same time, we highlight how these approaches can sustainably reduce your operating costs and lower CO₂ emissions.

  • Watch the educational video here
  • Find out more about data centres

RetroFIT+: Belimo's Assessment Tool for evaluating your building in accordance with the ISO 52120 standard (in German)

Duration: 17 minutes

With the RetroFIT+ Assessment Tool, you can evaluate project feasibility using key figures such as ROI, break-even point, and overall savings in energy, CO₂, and costs. This enables you to make well-founded decisions and provide decision-makers, consultants, operators, and partners (system integrators, plant manufacturers) with suitable methods and tools to quickly and easily determine the optimal solution for optimising the energy efficiency of property operations

  • Watch the educational video here
  • Learn more about the topic RetroFIT+

RetroFIT+ is a rapid and simple method for increasing energy efficiency in buildings (in German)

Duration: 33 minutes

With RetroFIT+, Belimo is providing decision makers, consultants, operators, and partners (system integrators, plant manufacturers) with suitable methods and tools for rapidly and easily determining ideal solutions for energy optimisation in real estate operations. In doing so, Belimo is not only communicating knowledge but also making experts available to lend support to the implementation process.

  • Watch the educational video here
  • Learn more about the topic RetroFIT+

Expert Talk: Latest IAQ findings in the fields of medicine, technology, and public policy (in German)

Duration: 52 minutes

In this educational video, leading experts illuminate the latest findings regarding indoor air quality (IAQ) and their wide-ranging effects on health, technologies, and general political conditions.
 

Speakers:

Prof. Dr. Adriano Aguzzi is Head of the Institute for Neuropathology at the University of Zurich. 

Claus Händel is Managing Director for Technology for the Fachverband Gebäude-Klima e.V. (FGK) [Professional Association for Building Climate Control]. 

Dr. Benoit Sicre is Head of the "Gesundheit und Hygiene im Gebäude" [Health and Hygiene in Buildings] research group at the Lucerne University of Applied Sciences and Arts – Technology & Architecture.

Mikko Gisin has been an Applications and Project Consultant for the last six years at BELIMO Automation AG and is an expert in sensors and ventilation systems. 

  • Watch the educational video here

Belimo ZoneEase™ VAV – Controlling of CO2, temperature, and volumetric flow (in German)

Duration: 24 minutes

Health, well-being, and productivity greatly depend on room climate. Therefore, good indoor air quality is fundamental to building design and operation. Variable volumetric flow controllers, also known as VAV, enable precise control of air volumetric flows via control sequences directly integrated into the VAV actuator.

Belimo ZoneEase™ VAV is an easy-to-operate VAV-based zone control ecosystem. The ZoneEase VAV solution simplifies the commissioning process. It provides commissioning and maintenance support via the cloud and smartphone to enhance the user experience and reduces project complexity and downtime while increasing connectivity, data transparency and cost-efficiency.

  • Watch the educational video here

Intelligent control butterfly valves (in German)

Duration: 38 minutes

Say goodbye to high energy consumption, inefficiency, discomfort, and sky-high costs caused by obsolete valves! Thanks to the innovative control butterfly valves from Belimo with nominal diameters from DN 100 to DN 300, these problems are now a thing of the past – just like the hassle of finding compatible Belimo RetroFIT+ solutions. 

Exactly what these solutions are and why they are such a game changer can be found in the following video tutorial, which focuses on the following points and questions:

  • Use of butterfly valves as control valves. How does Belimo manage to use intelligent butterfly valves as control valves?

  • What are the benefits and disadvantages of this solution and where can it be used?

  • How can control butterfly valves prove their worth over globe valves, and when is which technology appropriate?

  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

European Green Deal: Help! Or Hurrah!? (in German)

Duration: 23 minutes

The European Union's Green Deal has also had a concrete impact on the HVAC and technical building services sectors. But what exactly are the implications, and what can market participants and suppliers expect to happen? In this video tutorial, Belimo would like to address the following points and questions, among others: 

  • Overview of the regulatory landscape: What does the Green Deal mean for normative legislation such as the Energy Performance of Buildings Directive (EPBD), the Energy Performance of Buildings Act (EPBG) and the EU's taxonomy and criteria for sustainable economic activity in the context of Environmental Social Governance (ESG)?
  • Who will implement the agreed changes, who will be responsible for them, and who will be affected by the new Green Deal rules?
  • How will this work in practice? Belimo wants to show individual ways and solutions to answer these questions.  
  • Watch the educational video here

When do I need motorised fire dampers? (in German)

Duration: 30 minutes

Specialist planners and technical building services companies are often faced with the question of when fire dampers should be motorised as shut-off devices in ventilation systems. Unfortunately, in many cases, the approved fire protection concept does not provide specifics in this regard. "Where does it say that?" is one of the most frequently asked questions in this context.

The educational video looks at the different reasons for motorising fire dampers:

  • What does the legislator require in regulations such as the German Model Building Code (MBO) and specific building regulations?
  • What are the requirements of the German Model Ventilation System Guidelines (M-LüAR)?
  • What can be said about the generally accepted rules of technology?
  • What are the benefits of motorised fire dampers to the building owner?
  • Watch the educational video here

Belimo RetroFIT+ – Increasing energy efficiency in existing plants (in German)

Duration: 23 minutes

The existing air conditioning systems in existing buildings – heating, cooling and ventilation – often offer plenty of potential for energy savings. After all, intelligent control of heating, cooling and ventilation loads contributes significantly to the energy efficiency of buildings. Belimo has the right solution in its portfolio for these purposes and offers a comprehensive concept for increasing energy efficiency with the topic "RetroFIT+".

In this educational video, we present a Belimo task force that analyses existing systems and develops proposals for increasing efficiency, for example by using other hydronic circuits or pressure-independent valves. Find out which tools can achieve this and what role intelligent field devices such as the Energy Valve can play.

  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Distributors and hydronic circuits – basic training (in English)

Duration: 27 minutes

Which hydronic circuits are available? And which is the right one for my project? These questions are answered in the basic training, one of nine training courses on the topic of hydronics.

Six basic circuits cover more than 90 percent of applications. In this educational video you will learn more about these six circuits and their uses:

  • Throttling circuit
  • Injection circuit with 2-way valve
  • Mixing circuit
  • Mixing circuit with fixed pre-mixing
  • Diverting circuit
  • Injection circuit with 3-way valve
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Basic knowledge on the design of pressure-dependent valves: Part 1 (in English)

Duration: 14 minutes

How do I design pressure-dependent valves? What is an a-value? What is valve authority? These questions are the focus of this basic training 2.1.

The educational video covers basic knowledge on the design of pressure-dependent valves and focuses in particular on the following points:

  • Q = m x c x delta T
  • Variable-flow part of the circuit
  • A-value of heat exchangers
  • Kv/kvs values
  • Valve authority
  • Characteristic curve
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Indoor air quality and energy efficiency with AHUs (in English)

Duration 39 min.

HVAC systems are often installed with the aim of maintaining comfort levels in a building. However, less is usually known about the health benefits for building occupants and the energy efficiency of the building. By using central air handling units (AHUs) we address both the sustainability and indoor air quality aspects.

In this educational video, three of these factors are examined and discussed in more detail in relation to AHUs and energy efficiency.

  • Correct temperature and humidity conditioning
  • Effective filtration.
  • Proper amount of outdoor air
  • Watch the educational video here

Master 1: Thermal Energy Meter (TEM), recording, regulation and invoicing of heating and cooling (in English)

Duration: 32 minutes

How are heat/coolingmetersdesigned? What is a MID certification? What are position control, volumetric flow control and power control? What must be considered when reading meters, invoicing and calibration regulations? These questions are covered in master training 1.

The following contents are covered:

  • Thermal energy meter design (heat/cooling meter)
  • Introduction to the control concepts
    • Position control
    • Volumetric flow control
    • Power control
  • MID approval and calibration
  • Basic knowledge on the new heating cost regulations and calibration law
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Low delta T syndrome ─ causes and problems with low spread (in English)

Duration: 18 minutes

What is low delta T syndrome, and what causes it? How can it be rectified? How do we determine the correct delta T? Also, why have we used the delta T manager function in energy optimisation for years? These questions are the focus of this educational video.

The following contents are covered:

  • Reasons for low delta T syndrome
  • Optimisation of hydronics
  • Delta T manager ─ Function and type of action
  • Digital condition monitoring
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Basics 3.1: Basic knowledge on the design of pressure-independent valves (Part 1) (in English)

Duration: 20 minutes

What are the necessary fundamentals for professional design for pressure-independent valves? What are the different types? What needs to be considered? These questions are the focus of basic training 3.1.

The educational video covers basic knowledge on the design of pressure-independent valves and focuses in particular on the following points:

  • Function and design of pressure-independent control valves
  • Difference between mechanical/electronic
  • What does valve authority mean?
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Basics 3.2: Design of pressure-independent valves (Part 2) (in English)

Duration: 12 minutes

How are pressure-independent valves designed/dimensioned? What is valve authority? What should be considered? These questions are the focus of basic training 3.2.

The educational video covers basic knowledge on the design of pressure-independent valves and focuses in particular on the following points:

  • Design of pressure-independent control valves
  • Difference between mechanical/electronic
  • Valve authority
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Measurement concepts (in German)

Duration: 36 minutes

What does measurement concept, measurement point concept, and energy controlling mean? Why should the measurement concept be taken into account during hydronic planning? What are the contents of a measuring point concept? What are KPIs?

The educational video provides information on the integration of measurement concepts in hydronic planning and focuses in particular on the following points:

  • Measurement concepts for billing properties
  • Measurement concepts for energy controlling
  • Optimisation of measurement points
  • Energy data evaluation
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Special knowledge on hydronics and valves (in German)

Duration: 25 minutes

Are you already familiar with the basics of valves and hydronic circuits and now want to deepen your knowledge? Would you like to know more about the differences between globe valves and characterised control valves, about rangeabilities and the relevant characteristic curves? Then you've come to the right place with this educational video.

The seminar provides detailed knowledge for professionals focused in particular on the following points:

  • "Opening jump" of valves, cleaning of valve seat
  • Globe valve vs characterized ball valve
  • Valve characteristic curves
  • Rangeability
  • Cavitation
  • Information DIN EN 52120-1 (replacement DIN EN 15232-1)
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Consumption-based billing of energy costs for mechanical ventilation (in German)

Duration: 23 minutes

In commercial buildings with mechanical ventilation, it has been common practice for many years to allocate ventilation costs to the various occupants according to a pre-defined key. The distribution key used is usually the area allocated to each occupant relative to the total ventilated area of the building. However, this approach does not take into account or support newer trends and requirements to further reduce energy consumption in buildings.

What are the options available today for consumption-based billing of energy costs for mechanical ventilation? What is required by the Buildings Energy Act? What are the technical requirements? And when does consumption-based billing make economic sense?

These questions are the focus of this educational video.

The seminar will focus in particular on the following points:

  • Solutions for consumption-based billing of energy costs for mechanical ventilation
  • Buildings Energy Act and VDI 2077
  • Cost-effectiveness requirement for billing
  • Discussion of a cost allocation based on the actual volumetric flows in the distribution system

The educational video has been designed to be product-independent and generally valid, even if other manufacturers' products are used.

  • Watch the educational video here

Hydronic balancing and DIN EN ISO 52120-1 (in German)

Duration: 25 minutes

Are you already familiar with the basics of valves and hydronic circuits and now want to deepen your knowledge? Do you want to learn more about DIN EN ISO 52120-1 and what has changed with its introduction? 

The educational video provides detailed knowledge for professionals and focuses in particular on the following points:

  • Replacement of DIN EN 15232-1 by DIN EN ISO 52120-1
  • Consideration of hydronic balancing of heating and cooling systems
  • Energy efficiency classes
  • Consideration of residential buildings and non-residential buildings
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)

Specialised knowledge for zone solutions (in German)

Duration: 23 minutes

Are you already familiar with the basics of valves and hydronic circuits and now want to learn more? In this educational video, we introduce you to pressure-independent zone solutions in the 2-pipe and 4-pipe range. If you want to know what makes pressure-independent valves in the zone so special, what the benefits are for various applications and what solutions are available, you've come to the right place!

The seminar provides detailed knowledge for professionals focused in particular on the following points:

  • Differences between pressure-dependent and pressure-independent systems in the zone
  • 2-pipe and 4-pipe systems
  • Hydronic balancing in the zone
  • Pressure-independent quick compact valve PIQCV / 6-way valve EPIV
  • Watch the educational video here
  • Selection table of basic hydronic circuits (pdf - 1.09 MB)
Web-based training

To give you the highest flexibility and always keep track of your progress, you can complete the learning steps one by one and continue learning at a later time.
Please create a profile for this by registering.

Basic knowledge of sensors

Duration: 145 minutes

In this module series, we cover basic knowledge regarding sensors and answer the following questions:

  • Why are sensors so important in building automation?
  • What are their operating principles?
  • In which application areas are they used in the HVAC sector?
  • Start the learning path
  • Further information on this topic

Belimo Energy Valve™

Duration: 60 minutes

In this web-based training on our much sought-after energy valve with thermal energy meter, we cover the following topics:

  • What are the benefits of the energy valve?
  • Where is it used, and what control modes are possible?
  • What does low delta T syndrome mean, and how does the energy valve prevent this?
  • Start the learning path
  • Further information on this topic

Technology bus basics

Duration: 75 minutes

This basic training addresses the following questions about bus systems:

  • What is building topology?
  • What communication technologies are available?
  • Differences between building structures in the past, present and future
  • Which bus protocols are available at Belimo?
  • What are the benefits and disbenefits of the different bus protocols?
  • Start the learning path
  • Further information on this topic

Thermal energy meters

Duration: 150 minutes

In this web-based training, we teach the basics of our thermal energy meter with MID approval.

  • How our measuring principle works (heating/cooling)
  • How do we take into account and compensate for the glycol content in the water?
  • What communication interfaces and settings are available and possible via the web server?
  • Connection via NFC and operation with the Belimo Assistant
  • How is commissioning conducted?
  • How can I activate Power over Ethernet?
  • How can I activate the thermal energy meter?
  • What should be considered with the EN1434 and MID 2014/32/EU standards?
  • Start the learning path
  • Further information on this topic

Welcome to Belimo {{js-currentCountryName}}

{{js-currentCountryText}}
Contact Us Privacy Policy Change privacy settings Safety Notes Imprint
+2 0100 677 06 06
Subscribe to newsletter
BELIMO Egypt, 3 Omar Ibn Abd El Aziz Street, First 6th of October, Giza Governorate 3234126 (Egypt)